MFR4310 FlexRay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFR4310 FlexRay

1,747 Views
907439248
Contributor I

Hello, in the process of using MFR4310, channel A and B were configured in the tx slot, but in the actual work, channel A can communicate normally, but channel B has no data.The channel configuration and usage methods refer to the official routine.What might be the reason?Is it not supported by itself?

Labels (1)
0 Kudos
Reply
1 Reply

1,679 Views
nxa09859
NXP Employee
NXP Employee

Please check that the FlexRay controller is configured to work in the dual channel mode and that the channel B is enabled. Please, see the FR_MCR register for more details. Especially FR_MCR.SCM and FR_MCR.CHA and FR_MCR.CHB configuration.

0 Kudos
Reply