Hi,
I got two questions now of using S12ZVML for sensorless motor control.
1. for Delta connection, the Back-EMF constant calculation:
I measure the phase voltage at 1000rpm.Since phase voltage is equal to the line voltage,the constant in freemaster is Vpk(phase)/W(angleSpeed)? No need to divide sqrt(3)?
2. We use the external driver and interal current sense amplifier 0 for dc-bus current measurement.We left the HG/HS/VBS/VLS/LG/LS/LS0/CP/VCP all pins used by GDU unconnected.And enable the GDU ,and current sense amplifier 0. Howerever,the DC bus measurement value is bigger than the real value.
Is it ok to left these GDU relative PINs unconnected to just use the internal CSA?Or I need care about something else about the hardware design to use external driver?
Regards
Arrow
已解决! 转到解答。
Please provide more detail information about your application and the reason you need the external MOSFETs driver instead of internal one.
Here are comments to you question:
Please provide more detail information about your application and the reason you need the external MOSFETs driver instead of internal one.
Here are comments to you question: