I design the bootloader for 9S12G128 ,I need to remapping the interrupt vector table from 0xFF80-0xFFFF, I make some code like that(under words),the code can not work, when I reset ,the code can not enter into the main (); Is there where I need to set up?
#define __CPU_VECTOR_BASE_ADDR__ 0x7F80
/* ISR prototype */
typedef void (*near tIsrFunc)(void) ;
/*lint -save -e950 Disable MISRA rule (1.1) checking. */
#pragma CODE_SEG __NEAR_SEG NON_BANKED
interrupt void UnimplementedISR(void) //定义在NON_BANKED区
{}
void interrupt T0_inter(void)
{}
void interrupt T2_inter(void)
{}
void interrupt CAN_receive(void)
{}
#pragma CODE_SEG DEFAULT
static const tIsrFunc _InterruptVectorTable[] @__CPU_VECTOR_BASE_ADDR__ = {
/* Interrupt vector table */
/*put your ISR functions list here according to the interrupt vector order*/
&UnimplementedISR, /* vector 63 */
&UnimplementedISR, /* vector 62 */
&UnimplementedISR, /* vector 61 */
&UnimplementedISR, /* vector 60 */
&UnimplementedISR, /* vector 59 */
&UnimplementedISR, /* vector 58 */
&UnimplementedISR, /* vector 57 */
&UnimplementedISR, /* vector 56 */
&UnimplementedISR, /* vector 55 */
&UnimplementedISR, /* vector 54 */
&UnimplementedISR, /* vector 53 */
&UnimplementedISR, /* vector 52 */
&UnimplementedISR, /* vector 51 */
&UnimplementedISR, /* vector 50 */
&UnimplementedISR, /* vector 49 */
&UnimplementedISR, /* vector 48 */
&UnimplementedISR, /* vector 47 */
&UnimplementedISR, /* vector 46 */
&UnimplementedISR, /* vector 45 */
&UnimplementedISR, /* vector 44 */
&UnimplementedISR, /* vector 43 */
&UnimplementedISR, /* vector 42 */
&UnimplementedISR, /* vector 41 */
&UnimplementedISR, /* vector 40 */
&UnimplementedISR, /* vector 39 */
&CAN_receive, /* vector 38 */
&UnimplementedISR, /* vector 37 */
&UnimplementedISR, /* vector 36 */
&UnimplementedISR, /* vector 35 */
&UnimplementedISR, /* vector 34 */
&UnimplementedISR, /* vector 33 */
&UnimplementedISR, /* vector 32 */
&UnimplementedISR, /* vector 31 */
&UnimplementedISR, /* vector 30 */
&UnimplementedISR, /* vector 29 */
&UnimplementedISR, /* vector 28 */
&UnimplementedISR, /* vector 27 */
&UnimplementedISR, /* vector 26 */
&UnimplementedISR, /* vector 25 */
&UnimplementedISR, /* vector 24 */
&UnimplementedISR, /* vector 23 */
&UnimplementedISR, /* vector 22 */
&UnimplementedISR, /* vector 21 */
&UnimplementedISR, /* vector 20 */
&UnimplementedISR, /* vector 19 */
&UnimplementedISR, /* vector 18 */
&UnimplementedISR, /* vector 17 */
&UnimplementedISR, /* vector 16 */
&UnimplementedISR, /* vector 15 */
&UnimplementedISR, /* vector 14 */
&UnimplementedISR, /* vector 13 */
&UnimplementedISR, /* vector 12 */
&UnimplementedISR, /* vector 11 */
&T2_inter, /* vector 10 */
&UnimplementedISR, /* vector 09 */
&T0_inter, /* vector 08 */
&UnimplementedISR, /* vector 07 */
&UnimplementedISR, /* vector 06 */
&UnimplementedISR, /* vector 05 */
&UnimplementedISR, /* vector 04 */
&UnimplementedISR, /* vector 03 */
&UnimplementedISR, /* vector 02 */
&UnimplementedISR, /* vector 01 */
&UnimplementedISR, /* Reset vector */
};
void main(void)
{ IVBR = 0x7F;
//set the vector base
}
Is there where I need to set up?
已解决! 转到解答。
Hi,
It seems to be correct.
The attached example works on my side.
So please try it.
Regards,
Daniel
Hi,thank you for your help.There are still have some problems.
I open your example,I notice that you use" P&E USB BDM muitilink", I use "TBDML " download the program to MC9S12G128,But it can not works.What's wrong with it?Did you change the file,such as"project.prm" and"start12.c".
if MC9S12G128 connected with CW software,when I use the resert button in CW software,it can do well.
but,if I use buton in hardware reset ,it can't work,like that:
Regards,
Joy