I'm attempting to test a board with an MC9S12XEP100, using CodeWarrior version 5.1. Right now I'm just trying to compile and run a very simple test program, based on the Freescale example program. It compiles ok, and downloads ok to the XEP100, and I can examine memory and registers. BUT WHEN IT DOWNLOAD IN Uc IT SHOWS FOLLOWING LINES IN COMMAND WINDOW:-
STARTED
RUNNING
ILLEGAL_BP
And before this problem i had succesfully executed CAN,external MRAM,FLASH,SRAM program.but yesterday i am stuck in this prooblem. I've read most of the posts here about the "ILLEGAL_BP" message, and I'm not making any of the mistakes that others have reported;So please help me regarding this and please guide is this hardware problem or software??? so can make changes according to it.
Hi Aniket,
The ILLEGAL_BP error may be caused by a lot of reasons. The most of them described Edward in your second case ILLEGAL_BP with 9S12xep100
If you create, download and run a new project on the board did you see the same issue?
Could you share your code?
Some useful points can be seen in the document below.
I hope it helps you.
Best Regards,
Diana