FW: [S12 / MagniV Microcontrollers] - FW: LIN  assign frame ID range problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FW: [S12 / MagniV Microcontrollers] - FW: LIN  assign frame ID range problem

1,008件の閲覧回数
deepakchandra
Contributor III

Dear sir ,

Please help me out in below  problem its very urgent .

Sir, have to add  some additional  feature in our diagnostic class 2  as required by customer as listed below .

reset , information , hw vesion, sw version etc  i have to the use SID c6,c8 in our slave but i don't know how to do ,please suggest .

for example for reset .and information of ecu are listed below

 

 

 

 

 

From: Deepak Chandra 

Sent: 04 March 2016 10:01 AM

To: 'jive-1490806716-5tot-2-dasa@mail.freescale.jiveon.com'

Subject: RE:  - FW: LIN  assign frame ID range problem

 

1.now i have to add  some additional  feature in our diagnostic class 2  as required by customer as listed below .

reset , information , hw vesion, sw version etc  i have to the use SID c6,c8 in our slave but i don't know how to do ,please suggest .

for example for reset .and information of ecu are listed below

 

 

 

 

From: RadekS 

Sent: 02 March 2016 08:25 PM

To: deepak chandra

Subject: Re:  - FW: LIN  assign frame ID range problem

 

NXP Community

 

 

FW: LIN  assign frame ID range problem

reply from Radek Sestak in S12 / MagniV Microcontrollers - View the full discussion

 

 

 

Hi deepak,

 

Since this question/discussion is here twice, we could continue in just once:

https://community.freescale.com/thread/386513

 

Have a great day,

RadekS

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S12 / MagniV Microcontrollers by email or at NXP Community

Following FW: LIN  assign frame ID range problem in these streams: Inbox

 

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

ラベル(1)
1 返信

792件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi deepak,

Since this question/discussion is here twice, we could continue in just once:

https://community.freescale.com/thread/386513


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------