Analog to digital in EVB9S12NE64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Analog to digital in EVB9S12NE64

3,752 次查看
ibrahim2110
Contributor I
hi i've a problem with atd in EVB9S12NE64 i want to make the V refernce high to be 5volt (extrnaly)  instead of the 3.3 v supplied internaly by the kit
idon't know if the atd channels can withstand that 5volt
please if any one know how to do that reply me.
thanks for ur help
标签 (1)
0 项奖励
回复
2 回复数

806 次查看
EMontanez
NXP Employee
NXP Employee
For the NE64:

ATD references -

VRL: min = VSSA, max = VDDA/2
VRH: min = VDDA/2, max = VDDA

Where, VDDA: min = 3.135, max = 3.465. Therefore, a 5V ATD reference is not allowed. This kind of reference will cause internal diodes on these ATD pins to clamp.
0 项奖励
回复

806 次查看
peg
Senior Contributor IV
Hi,
The supply to the analogue section is generally the same voltage level as the main chips supply. (just cleaner hopefully)
If you want to measure voltages greater than this generally you use a resistive voltage divider into a rail-to-rail non-inverting op-amp connected to the ATD input.
The divider changes the 5V to 3 or so volts, then the buffer which is fed from the same analogue supply as the micros ADC section buffers it and provides a low source impedance to the ADC.
 
Hope that helps
Peg
0 项奖励
回复