Hello,
I´ve made this board below and I have testet the IO with the following code on each port (I used different Register names for each port):
LDAA #$00FF
STAA DDRB
Main:
LDAA #$00FF
STAA PORTB
JSR DELAY
LDAA #$0000
STAA PORTB
JSR DELAY
BRA Main
This works great but If I use bset or bclr instruction then it does not work. I am not able to toggle the led on my breadboard with the following code.)
Example:
BSET 0, DDRB ;also tried BSET DDRB, %00000001 without success and also the rest of the code in that way without success
Main:
BSET 0,PORTB
JSR DELAY
BCLR 0,PORTB
JSR DELAY
BRA Main
Can anyone help me?
I have to say, I am new to the 16Bit HCS MCU´s but I have a good knowledge on the HCS08. I always write my code in Assembly language.
-BR Ingo
解決済! 解決策の投稿を見る。
BSET DDRA, #0xFF will set all DDRA bits. HC08/S08 BSET instruction can set single bit, while S12 takes bit mask.
BSET 0, DDRA will probably set bit1 (DDRA address is 2, which is bitmask of bit1) of byte @0 (PORTA is at 0). Though it shouldn't even compile (in the right compiler), since immediate addressing requires # sign.
An example, for D32 in the CodeWarrior. You can find there also BSET and BCL instructions format.
;*******************************************************************************
;* Freescale Semiconductor Inc.
;* (c) Copyright 2004-2005 Freescale Semiconductor, Inc.
;* ALL RIGHTS RESERVED.
;*******************************************************************************
;Services performed by FREESCALE in this matter are performed AS IS and without
;any warranty. CUSTOMER retains the final decision relative to the total design
;and functionality of the end product. FREESCALE neither guarantees nor will be
;held liable by CUSTOMER for the success of this project.
;FREESCALE DISCLAIMS ALL WARRANTIES, EXPRESSED, IMPLIED OR STATUTORY INCLUDING,
;BUT NOT LIMITED TO, IMPLIED WARRANTY OF MERCHANTABILITY OR FITNESS FOR
;A PARTICULAR PURPOSE ON ANY HARDWARE, SOFTWARE OR ADVISE SUPPLIED TO THE PROJECT
;BY FREESCALE, AND OR NAY PRODUCT RESULTING FROM FREESCALE SERVICES. IN NO EVENT
;SHALL FREESCALE BE LIABLE FOR INCIDENTAL OR CONSEQUENTIAL DAMAGES ARISING OUT OF
;THIS AGREEMENT.
;
;CUSTOMER agrees to hold FREESCALE harmless against any and all claims demands or
;actions by anyone on account of any damage, or injury, whether commercial,
;contractual, or tortuous, rising directly or indirectly as a result of an advise
;or assistance supplied CUSTOMER in connection with product, services or goods
;supplied under this Agreement.
;*******************************************************************************
;* File main.c
;* Owner Ladislav
;* Version 1.0
;* Date Oct-4-2014
;* Classification General Business Information
;* Brief Test 8x8 CAN filter in loopback mode
;*******************************************************************************
; TECHNICAL SUPPORT - SOFTWARE EXAMPLE
;*******************************************************************************
;* Detailed Description:
;*
; - CAN0 in loopback mode
; - bitrate 250kbps
; - Used OSCCLK = 16MHz BUSCLK=8MHz, CANCLK derived from OSCCLK (recommended)
;
; The SW:
; 1) CAN0 Tx in polling mode CAN0 Rx is set for interrupt mode
;
; 2) Extended identifier is used only for Tx and Rx(filter)
;
; 3) Filters filter and accept all extended IDs only. Standard IDs are
; filtered out
; - tested on: EVB Softec ZK-S12-A
; - OSCCLK = 16MHz oscillator, BUSCLK = 8MHz
;*******************************************************************************
;Revision History:
;Version Date Author Description of Changes
;1.0 Oct-4-2014 Ladislav Initial version
; ******************************************************************************
; Include derivative-specific definitions
INCLUDE 'derivative.inc'
; export symbols
XDEF Entry, _Startup, main, CAN0RXISR
; we use export 'Entry' as symbol. This allows us to
; reference 'Entry' either in the linker .prm file
; or from C/C++ later on
XREF __SEG_END_SSTACK ; symbol defined by the linker for the end of the stack
;@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
; variable/data section
MY_EXTENDED_RAM: SECTION
; Insert here your data definition.
;extended ID structure
;0x00X0 IDR0 - ID28 ID27 ID26 ID25 ID24 ID23 ID22 ID21
;0x00X1 IDR1 - ID20 ID19 ID18 SRR(=1) IDE(=1) ID17 ID16 ID15
;0x00X2 IDR2 - ID14 ID13 ID12 ID11 ID10 ID9 ID8 ID7
;0x00X3 IDR3 - ID6 ID5 ID4 ID3 ID2 ID1 ID0 RTR
RXmsgID0 ds.b 1 ;
RXmsgID1 ds.b 1 ;
RXmsgID2 ds.b 1 ;
RXmsgID3 ds.b 1 ;
RXmsglen ds.b 1 ;
RXmsgdata0 ds.b 1
RXmsgdata1 ds.b 1
RXmsgdata2 ds.b 1
RXmsgdata3 ds.b 1
RXmsgdata4 ds.b 1
RXmsgdata5 ds.b 1
RXmsgdata6 ds.b 1
RXmsgdata7 ds.b 1
TXmsgID0 ds.b 1 ;
TXmsgID1 ds.b 1 ;
TXmsgID2 ds.b 1 ;
TXmsgID3 ds.b 1 ;
TXmsgprty ds.b 1 ;
TXmsglen ds.b 1 ;
TXmsgdata0 ds.b 1
TXmsgdata1 ds.b 1
TXmsgdata2 ds.b 1
TXmsgdata3 ds.b 1
TXmsgdata4 ds.b 1
TXmsgdata5 ds.b 1
TXmsgdata6 ds.b 1
TXmsgdata7 ds.b 1
data ds.b 1
tx_free_buf ds.b 1
;@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
; code section
MyCode: SECTION
main:
_Startup:
Entry:
LDS #__SEG_END_SSTACK ; initialize the stack pointer
;--------------------------
;data=1;
MOVB #1, data
;PEAR_NECLK = 0;
BCLR PEAR,#$10
;init CAN
;250 kbps, 1sample/bit, 16MHz ext osc as CAN clock source, loop disabled
;CAN interface (PCA82C250)
;init_CAN(0xC3, 0x67, CAN0CTL1_CANE_MASK | CAN0CTL1_LOOPB_MASK);
;CAN0CTL0 = CAN0CTL0_INITRQ_MASK;
MOVB #1, CAN0CTL0
;while(!(CAN0CTL1 & CAN0CTL1_INITAK_MASK));
BRCLR CAN0CTL1,#1,*+0
;CAN0CTL1 = CAN0CTL1_CANE_MASK | CAN0CTL1_LOOPB_MASK;
;Enables MSCAN, Oscillator Clock, Loop Enabled/Disabled and Normal Operation
MOVB #$A0,CAN0CTL1
;CAN0BTR0 = 0xC3;
MOVB #$C3, CAN0BTR0
;CAN0BTR1 = 0x67;
MOVB #$67, CAN0BTR1
;CAN0IDAC = 0x10; // CAN Filter 4x16
MOVB #$10, CAN0IDAC
; ACCEPT ALL EXTENDED IDs
; 16b CAN Filter scheme for extended identifier
; ID28 ID27 ID26 ID25 ID24 ID23 ID22 ID21
; ID20 ID19 ID18 SRR(=1) IDE(=1) ID17 ID16 ID15
;CAN0IDAR0_CAN0IDAR1 = 0x0008; // extended ID flag
MOVW #$0018, CAN0IDAR0 ; SRR=1, IDE=1
;CAN0IDMR0_CAN0IDMR1 = 0xFFE7; // accept extended identifiers only
MOVW #$FFE7,CAN0IDMR0 ; check SRR and IDE
;CAN0IDAR2_CAN0IDAR3 = 0x0008; // extended ID flag
MOVW #$0018, CAN0IDAR2 ; SRR=1, IDE=1
;CAN0IDMR2_CAN0IDMR3 = 0xFFE7; // accept extended identifiers only
MOVW #$FFE7,CAN0IDMR2 ; check SRR and IDE
;CAN0IDAR4_CAN0IDAR5 = 0x0008; // extended ID flag
MOVW #$0018, CAN0IDAR4 ; SRR=1, IDE=1
;CAN0IDMR4_CAN0IDMR5 = 0xFFE7; // accept extended identifiers only
MOVW #$FFE7,CAN0IDMR4 ; check SRR and IDE
;CAN0IDAR6_CAN0IDAR7 = 0x0008; // extended ID flag
MOVW #$0018, CAN0IDAR6 ; SRR=1, IDE=1
;CAN0IDMR6_CAN0IDMR7 = 0xFFE7; // accept extended identifiers only
MOVW #$FFE7,CAN0IDMR6 ; check SRR and IDE
;CAN0TL0 = 0x00; // restart MSCAN peripheral
CLR CAN0CTL0
;while(CAN0CTL1_INITAK); // wait for Initialization Mode exit
BRSET CAN0CTL1,#1,*+0
;while(!CAN0CTL0_SYNCH); // waits for MSCAN synchronization with the CAN bus
BRCLR CAN0CTL0,#16,*+0
;CAN0RIER_RXFIE = 1; // enable can 0 Rx interrupt
BSET CAN0RIER,#1
;EnableInterrupts;
CLI
;---------------------------------------
EndlessLoop:
;--- prepare CAN Tx frame ---
;TXmsgID = 0x12183456; only example but SRR and IDE must be 1 for extended ID
;extended ID structure
;IDR0 - ID28 ID27 ID26 ID25 ID24 ID23 ID22 ID21
;IDR1 - ID20 ID19 ID18 SRR(=1) IDE(=1) ID17 ID16 ID15
;IDR2 - ID14 ID13 ID12 ID11 ID10 ID9 ID8 ID7
;IDR3 - ID6 ID5 ID4 ID3 ID2 ID1 ID0 RTR
MOVB #$12,TXmsgID0
MOVB #$18,TXmsgID1 ; SRR=1, IDE=1
MOVB #$34,TXmsgID2
MOVB #$56,TXmsgID3
;TXmsglen = 8;
MOVB #8,TXmsglen
;TXmsgprty= 3;
MOVB #3,TXmsgprty
;TXmsgdata0_7= data++;
LDAB data
STAB TXmsgdata0
INCB
STAB TXmsgdata1
INCB
STAB TXmsgdata2
INCB
STAB TXmsgdata3
INCB
STAB TXmsgdata4
INCB
STAB TXmsgdata5
INCB
STAB TXmsgdata6
INCB
STAB TXmsgdata7
INCB
STAB data
;---use prepared data and fill can registers ---
;find free Tx buffer
;tx_free_buf = 0;
CLR tx_free_buf
;while(!(CAN0TFLG & (0x01<<tbuf_n_empty_flag))) // find empty transmit buffer from 3 buffers
MAINLBL2:
MOVB #1, tx_free_buf
BRSET CAN0TFLG,#1,MAINLBL1
MOVB #2, tx_free_buf
BRSET CAN0TFLG,#2,MAINLBL1
MOVB #4, tx_free_buf
BRSET CAN0TFLG,#4,MAINLBL1
JMP MAINLBL2
MAINLBL1:
;CAN0TBSEL = 0x01 << tbuf_n_empty_flag; // select found empty transmit buffer
MOVB tx_free_buf,CAN0TBSEL
;fill Tx ID
MOVB TXmsgID0,CAN0TXIDR0
MOVB TXmsgID1,CAN0TXIDR1
MOVB TXmsgID2,CAN0TXIDR2
MOVB TXmsgID3,CAN0TXIDR3
;fill Tx data buffers
MOVB TXmsgdata0,CAN0TXDSR0
MOVB TXmsgdata1,CAN0TXDSR1
MOVB TXmsgdata2,CAN0TXDSR2
MOVB TXmsgdata3,CAN0TXDSR3
MOVB TXmsgdata4,CAN0TXDSR4
MOVB TXmsgdata5,CAN0TXDSR5
MOVB TXmsgdata6,CAN0TXDSR6
MOVB TXmsgdata7,CAN0TXDSR7
;CAN0TXDLR = TXmsglen; // set message data length
MOVB TXmsglen, CAN0TXDLR
;CAN0TXTBPR = TXmsgprty; // set message internal priority
MOVB TXmsgprty, CAN0TXTBPR
;CAN0TFLG = (0x01<<tbuf_n_empty_flag); // clear flag to send message
MOVB tx_free_buf,CAN0TFLG
;-------------------------
BSR DELAY
;-------------------------
JMP EndlessLoop ; restart.
;"""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
DELAY:
;"""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
;for(i=0;i<0x05;i++) for(j=0;j<0xFFFF;j++) { asm nop; }
PSHD
PSHX
LDD #5
DELAYLBL1:
LDX #$FFFF
DELAYLBL2:
NOP
DBNE X,DELAYLBL2
DBNE D,DELAYLBL1
PULX
PULD
RTS
;"""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
CAN0RXISR: ; here is one of possible approaches to connect interrupt vector
; with label(address)
; 1) see export symbols on the top of this page
; 2) see vector definition in the Project.prm file (bottom):
; VECTOR 38 CAN0RXISR
;
;"""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
MOVB CAN0RXIDR0,RXmsgID0
MOVB CAN0RXIDR1,RXmsgID1
MOVB CAN0RXIDR2,RXmsgID2
MOVB CAN0RXIDR3,RXmsgID3
;RXmsglen = CAN0RXDLR & 0x0F;
LDAB CAN0RXDLR
ANDB #15
STAB RXmsglen
;RXmsgdata0_7 = CAN0RXDSR0_7;
MOVB CAN0RXDSR0,RXmsgdata0
MOVB CAN0RXDSR1,RXmsgdata1
MOVB CAN0RXDSR2,RXmsgdata2
MOVB CAN0RXDSR3,RXmsgdata3
MOVB CAN0RXDSR4,RXmsgdata4
MOVB CAN0RXDSR5,RXmsgdata5
MOVB CAN0RXDSR6,RXmsgdata6
MOVB CAN0RXDSR7,RXmsgdata7
;CAN0RFLG = CAN0RFLG_RXF_MASK; // clear flag
MOVB #1,CAN0RFLG
RTI
;@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
Best regards,
Ladislav
Thanks for your help!
I am sorry, I was so blind and could´nt see that
BSET PORTB,mDDRB_BIT7
BCLR PORTB,mDDRB_BIT7
works perfectly for me!
Now I am trying to determine the Busclock with an Frequency Counter. Pin PE7 is tied to ground (Pierce Oscillator 16Mhz 2pcs. 22pF).
Everything I am trying Ends up with a 137khz Busclock and I dont know how to fix it.
This is my schematic:
Can anyone help me out? I would like to have a 8Mhz or 16 Mhz busclock.
BR
-Ingo
Hi,
the PLL components you use are the most suitable for PLL setup with Synr=refdv=10 when you want to make 16MHz busclk from a S12 MHz oscclk. I suppose you have used correct load capacitance for used oscillator.
E256 : input pin capacitance for pins XTAL, EXTAL C1i = C2i = 7pF = Ci
Let C3=C4 = Ce
CLoad = (Ci + Ce)/2 and it has to be >= CLoad = 10 pF Cload is taken from a datashett for given oscillator, in this example 10pF
Then:
(Ci + Ce)/2 >= CL => Ce >= CL*2 - Ci
Ce >= 10pF * 2 - 7pF
Ce >= 13 pF
Rb value is from the interval 100kohm ~ 20Mohm. For low frequency circuits is crystal impedance relatively high and Rb should be high Rb = 10Mohm. For high frequencies (>20Mhz) Rb = 100 kohm.
Rs for high frequencies (>4MHz) can be omitted.
Moreover I suppose that you have only 100nF capacitors between Vdd and Vss because some customers connected Vdd to 5V which is mistake. May I see entire environment of the MCU?
Simple example of PLL setup:
static void PLL_Init(void)
{
CLKSEL &= 0x7F; // set BUS CLOCK 16MHz from 16MHz MHz OSCCLK
REFDV = 0;
SYNR = 0;
while(!(CRGFLG_LOCK));
CLKSEL_PLLSEL = 1;
PEAR_NECLK = 0; // make BUSCLK visible at PE4 pin
}
Have you measure frequency at oscillator to be sure it is working?
I hope you do not have any wire nor ground plane under oscillator circuitry. It can affect the oscillator in the way it is not working.
I would like to ask you, in the future, to create a new question at community if it does not corresponds to previous question.
Best regrads,
Ladislav
BSET DDRA, #0xFF will set all DDRA bits. HC08/S08 BSET instruction can set single bit, while S12 takes bit mask.
BSET 0, DDRA will probably set bit1 (DDRA address is 2, which is bitmask of bit1) of byte @0 (PORTA is at 0). Though it shouldn't even compile (in the right compiler), since immediate addressing requires # sign.