LWE has not been supported in the latest SDK release, you can find LWE in the previous Ltib release ISO http://www.freescale.com/webapp/sps/download/license.jsp?colCode=QORIQ_SDK_B2.03&prodCode=P4080PCIE&....
Yiping,
I already have lwe_apps source and I am saying I was able to run Hello World application just fine. I tried modifying hello world application and tried creating a new binary and that worked too. I am getting errors whenever I try to use ncurses.h library functions(for ex- initscr, endwin etc). I am pasting part of the error I am seeing below -
hello.o: In function `main':
hello.c:(.text+0xc): undefined reference to `initscr'
hello.c:(.text+0x2c): undefined reference to `endwin'
collect2: ld returned 1 exit status
make[2]: *** [hello.elf] Error 1
make[2]: Leaving directory `/home/lahar/Downloads/ltib/ltib-e500mc-20110128/rpm/BUILD/lwe_apps-b2.3/hello/dp'
make[1]: *** [all] Error 2
make[1]: Leaving directory `/home/lahar/Downloads/ltib/ltib-e500mc-20110128/rpm/BUILD/lwe_apps-b2.3/hello'
make: *** [hello] Error 2
error: Bad exit status from /home/lahar/Downloads/ltib/ltib-e500mc-20110128/tmp/rpm-tmp.29061 (%build)
RPM build errors:
Bad exit status from /home/lahar/Downloads/ltib/ltib-e500mc-20110128/tmp/rpm-tmp.29061 (%build)
Build time for lwe_apps: 1 seconds
Failed building lwe_apps
f_scbuild() returned an error, exiting
traceback:
main:561
LWE has not been supported in the latest SDK release, you can find LWE in the previous Ltib release ISO http://www.freescale.com/webapp/sps/download/license.jsp?colCode=QORIQ_SDK_B2.03&prodCode=P4080PCIE&....
Thanks Yiping. Really appreciate your help!
I have one more question - I explored all the docs from the ltib package(including doxygen files) but I am having hard time figuring out how to create an LWE application. Could you please direct me to the right path?
LWE_Applications_User_Manual.pdf mostly talks about example applications. It doesn't really provide directions for a new one. Anyway I have created a basic C application. It runs fine on my computer. I was able to compile and run using gcc. But whenever I try to build that application using ltib (./ltib -m scbuild -p lwe_apps) I get an error saying "No such file or directory found" I am getting this error for most of the libraries for ex - iostream and ncureses. I am assuming the problem is the path to the libraries but I am not sure how and where to fix the path for these libraries. could you please help? Thank you very much for your help!
Please execute "./ltib -c", and select lwe and lwe_apps, which have been selected by default, then build these packages with ltib automatically. After generating the rootfs filesystem, lwe are put in /opt folder in rootfs.
Thank you very much for replying Yiping!
I was able to run hello world application just fine. So, I have understanding of how to build and run an application. My question is "how to use an external library" for LWE application? meaning libraries used by LWE applications reside under rootfs/usr/include/ directory. If I need a library(for ex- ncurses.h etc) that doesn't reside under rootfs/usr/include directory. How do I add that? I can not manually moved a library file inside this directory because this directory doesn't provide us permissions to do so. Would it be fine if I change the permissions of the directory and try to move a file in there manually?
Or should I try to modify makefile for this?
Just wondering is there any documentation on this?
Thanks!