Has anyone successfully built the fsl-image-lsb-sdk bitbake image using the 1.3 SDK?
I installed yocto from the 1.3 (20121114) SDK iso, on a fresh install of Ubuntu 12.04.2 LTS. Now I know that 12.04.1 (and 12.04) are explicitly supported and 12.04.2 is not explicitly supported, but this is not a platform problem as far as I can tell.
Bitbake notices an error during dependency checking at the beginning of the build:
NOTE: Preparing runqueue
ERROR: Multiple .bb files are due to be built which each provide udev (/home/dvb/QorIQ-SDK-V1.3-20121114-yocto/meta/recipes-core/udev/udev_164.bb /home/dvb/QorIQ-SDK-V1.3-20121114-yocto/meta-oe/meta-oe/recipes-core/udev/udev_182.bb).
This usually means one provides something the other doesn't and should.
This problem comes back to bite me during the build, as the 182 udev is needed (actually udev >=172) by the recipe systemd-git-r29.
checking for UDEV... no
| configure: error: Package requirements ( libudev >= 172 ) were not met:
|
| Requested 'libudev >= 172' but version of libudev is 164
|
| Consider adjusting the PKG_CONFIG_PATH environment variable if you
| installed software in a non-standard prefix.
|
| Alternatively, you may set the environment variables UDEV_CFLAGS
| and UDEV_LIBS to avoid the need to call pkg-config.
| See the pkg-config man page for more details.
| ERROR: oe_runconf failed
NOTE: package systemd-git-r29: task do_configure: Failed
What is the correct way to work around this problem?
Note that fsl-image-minimal builds correctly. I have not yet tested deploying it on a box but the build completed without error.
One other thing I noted was that the "distro" field output by Yocto at the beginning of the build is 1.2 not 1.3, though I may be confusing things here:
OE Build Configuration:
BB_VERSION = "1.15.2"
TARGET_ARCH = "powerpc"
TARGET_OS = "linux"
MACHINE = "p2041rdb"
DISTRO = "fsl"
DISTRO_VERSION = "1.2"
TUNE_FEATURES = "m32 fpu-hard ppce500mc"
TARGET_FPU = "hard"
meta
meta-yocto = "master:b936b3333997d36d401a9c6a9603af57fc88e842"
meta-fsl-ppc = "master:0e12f1d72e778d98a0e2d7cf2c9df09b545d40d9"
meta-fsl-ppc-private = "(nobranch):4e71da366b990d4861c5f64fcf071152c8d2a32f"
meta-oe = "master:4f9dd3e80eb59c7c73841c85a2a703b98566572c"
解決済! 解決策の投稿を見る。
Regarding the build issue of fsl-image-lsb-sdk, you can try following workaround:
1. edit meta-fsl-ppc/conf/machine/p2041rdb.conf to add PREFERRED_VERSION_udev="175"
2. bitbake udev -c cleansstate
3. bitbake fsl-image-lsb-sdk
The distro version is Yocto version instead of FSL SDK version, SDK 1.3 uses Yocto 1.2.
BTW, since fsl-image-lsb-sdk includes the packages of lsb standard, the rootfs image size is very large, and most packages are not necessary, fsl-image-core/fsl-image-full are recommended rootfs types.
Regarding the build issue of fsl-image-lsb-sdk, you can try following workaround:
1. edit meta-fsl-ppc/conf/machine/p2041rdb.conf to add PREFERRED_VERSION_udev="175"
2. bitbake udev -c cleansstate
3. bitbake fsl-image-lsb-sdk
The distro version is Yocto version instead of FSL SDK version, SDK 1.3 uses Yocto 1.2.
BTW, since fsl-image-lsb-sdk includes the packages of lsb standard, the rootfs image size is very large, and most packages are not necessary, fsl-image-core/fsl-image-full are recommended rootfs types.
Thanks for the tip, it's building now and got past the udev breakage I saw
earlier. I'll mark this as answered as soon as the build completes.
On Fri, Mar 29, 2013 at 6:51 PM, Zhenhua Luo