U-boot prompt not coming in T4240 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot prompt not coming in T4240 board

988件の閲覧回数
smitagumansingh
Contributor I

Hi ,

Unfortunately my T4240 board got bricked and I am unable to get u-boot prompt. Please help me to unbrick my T4240 board .

0 件の賞賛
返信
5 返答(返信)

830件の閲覧回数
smitagumansingh
Contributor I

Hi Ufedor,

I have installed CodeWarrior on my window machine but unable to perform NOR Flash from the ISO image. Is there any document or QSG to follow flashing of an image using CodeWarrior  USB TAB ?

0 件の賞賛
返信

830件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the following section in the SDK Documentation:

Submit Form 

0 件の賞賛
返信

830件の閲覧回数
ufedor
NXP Employee
NXP Employee

If the board is T4240RDB you can try to boot from the alternative NOR Flash bank by setting SW3(3:1)=OFF-ON-ON.

0 件の賞賛
返信

830件の閲覧回数
smitagumansingh
Contributor I

Hi Ufedor,

Thanks for the quick reply. I tried by changing SW3 switch setting to SW3(3:1)=OFF-ON-ON , still u-boot prompt is not coming. Any other way to get it back ??

0 件の賞賛
返信

830件の閲覧回数
ufedor
NXP Employee
NXP Employee

In this case it is required to use CodeWarrior Flash Programmer to restore complete NOR Flash from the image provided in the SDK Source ISO availabled at:

https://freescaleesd.flexnetoperations.com/337170/477/10318477/QorIQ%20Linux%20SDK%20v2.0%20PPC64E65... 

0 件の賞賛
返信