Thermal managment on QorlQ devices for Boundary Scan

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Thermal managment on QorlQ devices for Boundary Scan

505 次查看
kirillmakhotin
Contributor I

We use QorlQ devices in our design (LS1020 and T1040). We want to use boundary scan testing after production assembly on smt line. Can we manage thermal levels of this devices when we apply power to boards to do boundary scan? Our development team give me (test eingineer) prototype of the board, but it heats up when i power it, even if it doesn't have any configuration and working program on it. After technological tests before functional control we attache heatsink to board, but it is not so comfortable to do it before boundary scan, espeacially if we need to do repair steps.

标记 (2)
0 项奖励
回复
1 回复

450 次查看
ufedor
NXP Employee
NXP Employee

Even with PORESET_B asserted power consumption is significant.

Estimated numbers are:

LS1020A - 1.0-1.2 W

T1040 - 2.2-2.5 W

Thus the boundary scan testing can be performed only with attached heatsinks.

0 项奖励
回复