T2080QDS vs. T2080RDB-PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080QDS vs. T2080RDB-PC

2,730件の閲覧回数
sharad_patel
Contributor II

What is the major differences between T2080QDS and T2080RDB-PC board?

I am discussing this boards with one of the mutual customer. The price difference is huge so he wants to understand the difference between the two boards.

Thank you,
Sharad

5 返答(返信)

2,385件の閲覧回数
sharad_patel
Contributor II

Thanks. I appreciate the confirmation. Main goal was to find out if T2080QDS version is still manufactured and supported, and so user is free to decide to buy either of T2080QDS or T2080RDB based on his/her need.

0 件の賞賛
返信

2,385件の閲覧回数
ufedor
NXP Employee
NXP Employee

In general the T2080QDS is more versatile in SerDes lanes connection, also it has Nexus/Aurora link (which is not implemented on the T2080RDB-PC).

In turn the T2080RDB-PC has C293 coprocessor and can be used as PCIe add-in card.

Please refer to the attached brief documents for the boards.

2,385件の閲覧回数
sharad_patel
Contributor II

Does NXP manufactures T2080QDS or they stopped manufacturing it?

Which is the latest version of these two boards?

0 件の賞賛
返信

2,385件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Both T2080QDS-PA and T2080RDB-PC are active and supported products.

T2080QDS-PA Product Information|NXP 

T2080RDB-PC Product Information|NXP 

0 件の賞賛
返信

2,385件の閲覧回数
ufedor
NXP Employee
NXP Employee

The latest revisions are T2080QDS-PA and T2080RDB-PC.

You wrote:

> Does NXP manufactures T2080QDS or they stopped manufacturing it?

What is the rationale of the question?