P2020 x MPC8641D Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 x MPC8641D Power

Jump to solution
1,292 Views
victorjardim
Contributor I

Hello all,

I'm evaluating the processors P2020 and MPC8641D, for choosing one of them for a new project. I´ve noticed that P2020 power consuption is like one fifth of the MPC8641D consuption, at the same core frequency and same core voltage. Is this right? How could you achieve such a huge power decreasement?

Thanks

Victor

0 Kudos
Reply
1 Solution
1,157 Views
lunminliang
NXP Employee
NXP Employee

They have different technolgy, MPC8641D is 90nm silicon-on-insulator(SOI), while P2020 is on 45 nm technology low-power platform.

View solution in original post

0 Kudos
Reply
1 Reply
1,158 Views
lunminliang
NXP Employee
NXP Employee

They have different technolgy, MPC8641D is 90nm silicon-on-insulator(SOI), while P2020 is on 45 nm technology low-power platform.

0 Kudos
Reply