NXP's Reference Design Board is not using the SD Card Kernel Image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP's Reference Design Board is not using the SD Card Kernel Image

472件の閲覧回数
jaytirthkhairat
Contributor I

I am working on NXP LS2088A RDB. The RDB comes pre-loaded with software. The software is loaded in NOR flash on the RDB. When the power button on the front of the chassis is pressed the U-boot loader automatically runs and then loads and starts Linux using images located in vbank0 of the RDB's NOR flash. Following are the details of the default Linux:

 :~# uname -r
  4.1.8-rt8+gca03abf   
 :~# cat /etc/version
  20161221131900

The /boot directory is empty.

Now, the RDB provides an option of booting using an SD card linux. I have a bootable SD card with Linux kernel 4.1.8-rt8+g9873f6b (created using YOCTO images and bitbake). I followed the instructions in the manual and booted the RDB with this SD card. I executed the commands mentioned above. Following are the details:

 :~# uname -r
  4.1.8-rt8+gca03abf   
 :~# cat /etc/version
  20170727103535

The /boot directory contains the file Image-4.1.8-rt8+g9873f6b (i.e the kernel image in the SD card) along with other dtb and link files. I am unable to understand why the uname -r is still showing the default RDB kernel version? Why is the SD card kernel image not used by the RDB although it is using the file system?

タグ(1)
0 件の賞賛
返信
0 返答(返信)