LS2088A BSDL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088A BSDL

820件の閲覧回数
rodrigobernardo
Contributor I

 Hello...

I'm working in the product Test Coverage analysis and I have to analyze the Coverage of the Product with LS2088A device that will be tested using ##IEEE 1149 boundary Scan Standard Test.

This BSDL will be Grateful to have, in order to have the accurate analysis and Boundary Scan Test Application.

0 件の賞賛
返信
1 返信

718件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The BSDL and can be provided under non-disclosure agreement (NDA) only. To obtain additional information please create a Technical Case:

https://community.nxp.com/thread/381898

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信