[LS1046A][DPAA1] VLAN PCP header manipulation update elements fill and index?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1046A][DPAA1] VLAN PCP header manipulation update elements fill and index?

ソリューションへジャンプ
1,872件の閲覧回数
alance
Contributor II

Hi

We'd like to use DPAA1 header manipulation update to set VLAN PCP header. From the document, it is set from dscp elements fill and index. Could you provide more info about how these elements map to VLAN PCP? Thanks.  

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-40D0A317-2C60-411F-B...

 

0 件の賞賛
返信
1 解決策
1,855件の閲覧回数
bpe
NXP Employee
NXP Employee

If what you want is just to set a new PCP value in the outer VLAN tag, use
type="vpri", not "dscp".

DSCP in DPAA1 header manipulation establishes a mapping between IP TOS field and
the priority field in the VLAN tag, so the frame must encapsulate a valid IP datagram.
If that is what yo want, study LS1046ADPAARM, Sections 5.12.10.8 and 5.12.10.8.1
to have an idea of the array the document you referred talks about.

Hope this helps,
Platon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,856件の閲覧回数
bpe
NXP Employee
NXP Employee

If what you want is just to set a new PCP value in the outer VLAN tag, use
type="vpri", not "dscp".

DSCP in DPAA1 header manipulation establishes a mapping between IP TOS field and
the priority field in the VLAN tag, so the frame must encapsulate a valid IP datagram.
If that is what yo want, study LS1046ADPAARM, Sections 5.12.10.8 and 5.12.10.8.1
to have an idea of the array the document you referred talks about.

Hope this helps,
Platon

0 件の賞賛
返信