LS1043ardb serdes interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043ardb serdes interface

跳至解决方案
1,071 次查看
akeshchacko
Contributor II

hi,

we are currently working on ls1043ardb reference board with SDK0.5. When using RCW 4555 (req. for our target board) it is not able to detect mPCIe card in the reference board. Changed the PLL1 clock frequency to 100MHz (by changing SD1REFCLK_SEL switch to 0). We are using SD card booting. Are we missing something?? Given below is the RCW configuration.

# RCW

08100010 0a000000 00000000 00000000

45550002 80004012 60040000 c1002000

00000000 00000000 00000000 00038800

00000000 00001100 00000096 00000001

标记 (1)
0 项奖励
回复
1 解答
887 次查看
ufedor
NXP Employee
NXP Employee

For the 100MHz reference clock value of the RCW bit SRDS_PLL_REF_CLK_SEL_Sn - SerDes PLL1 (RCW[160]) has to be 0, but it is 1 in the provided RCW.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
888 次查看
ufedor
NXP Employee
NXP Employee

For the 100MHz reference clock value of the RCW bit SRDS_PLL_REF_CLK_SEL_Sn - SerDes PLL1 (RCW[160]) has to be 0, but it is 1 in the provided RCW.

0 项奖励
回复
887 次查看
nikhilprakash
Contributor IV

Thanks ufedor.We will try with the changed rcw.

0 项奖励
回复