LS1043ARDB does it support ebtables

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB does it support ebtables

Jump to solution
678 Views
abhijeet_sasmal
Contributor I

Does it support ebtables?

0 Kudos
Reply
1 Solution
618 Views
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
619 Views
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply