LS1043ARDB does it support ebtables

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043ARDB does it support ebtables

跳至解决方案
676 次查看
abhijeet_sasmal
Contributor I

Does it support ebtables?

0 项奖励
回复
1 解答
616 次查看
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
617 次查看
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复