LS1043A-CONNECT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A-CONNECT

1,174 Views
肆加贰
Contributor I

ARM板连接情况.JPG

We use the core board of the LS1043A chip. After power-on, the power supply part is normal. After connecting the CodeWarrior TAP and clicking the A button in the figure, the error in the B area will appear. Our hardware has an error in design, CFG_RCW_SRC0-8 floating, will this hardware error cause this error? Is it possible to modify the Target Initialization file so that the debugger can connect successfully and then debug normally?

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies