Is there a PROFINET IRT solution with QorIQ chips available without using an external ASIC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a PROFINET IRT solution with QorIQ chips available without using an external ASIC?

Jump to solution
2,131 Views
h_theo
Contributor I

I'm interested in realizing a PROFINET IRT (conformance class C) device with minimal HW costs. Theirfore I apreciate using a QorIQ without external ASIC. Is there a solution from Freescale or partner available?

1 Solution
1,868 Views
lunminliang
NXP Employee
NXP Employee

Hi h.theo


Even though we do not have single chip solution for PROFINET IRT solution, we have two chip solution with HMS engagement, which do not need external ASIC. We’re working on the demo for this. If you’re interested, we can provide more details later.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
1,868 Views
donikuy
Contributor III

Hi Lunmin,

I would also be interested in the HMS Profinet solution.

Could you please provide me with some information?

Kind Regards,

Ylber Doniku

0 Kudos
Reply
1,868 Views
lunminliang
NXP Employee
NXP Employee

Hi

Freescale Profinet webpage for your information:

PROFINET|Freescale

Regards

Lunmin

0 Kudos
Reply
1,868 Views
h_theo
Contributor I

Hi,

thank you for your response. I already visited that page and found only information about PROFINET. But there is not mentioned wether PROFINET IRT or RT is supported, e.g. by using the QUICC engine or the like. Also the mentioned partners show solutions only for PROFINET RT but not IRT (except those demanding external ASICs).

Regards

Hannen

0 Kudos
Reply
1,869 Views
lunminliang
NXP Employee
NXP Employee

Hi h.theo


Even though we do not have single chip solution for PROFINET IRT solution, we have two chip solution with HMS engagement, which do not need external ASIC. We’re working on the demo for this. If you’re interested, we can provide more details later.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,868 Views
donikuy
Contributor III

Hi Lunmin,

I would also be interested in the HMS Profinet solution.

Could you please provide me with some information?

Kind Regards,

Ylber Doniku

0 Kudos
Reply