Is there a PROFINET IRT solution with QorIQ chips available without using an external ASIC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a PROFINET IRT solution with QorIQ chips available without using an external ASIC?

ソリューションへジャンプ
1,775件の閲覧回数
h_theo
Contributor I

I'm interested in realizing a PROFINET IRT (conformance class C) device with minimal HW costs. Theirfore I apreciate using a QorIQ without external ASIC. Is there a solution from Freescale or partner available?

1 解決策
1,512件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi h.theo


Even though we do not have single chip solution for PROFINET IRT solution, we have two chip solution with HMS engagement, which do not need external ASIC. We’re working on the demo for this. If you’re interested, we can provide more details later.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
1,512件の閲覧回数
donikuy
Contributor III

Hi Lunmin,

I would also be interested in the HMS Profinet solution.

Could you please provide me with some information?

Kind Regards,

Ylber Doniku

0 件の賞賛
返信
1,512件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi

Freescale Profinet webpage for your information:

PROFINET|Freescale

Regards

Lunmin

0 件の賞賛
返信
1,512件の閲覧回数
h_theo
Contributor I

Hi,

thank you for your response. I already visited that page and found only information about PROFINET. But there is not mentioned wether PROFINET IRT or RT is supported, e.g. by using the QUICC engine or the like. Also the mentioned partners show solutions only for PROFINET RT but not IRT (except those demanding external ASICs).

Regards

Hannen

0 件の賞賛
返信
1,513件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi h.theo


Even though we do not have single chip solution for PROFINET IRT solution, we have two chip solution with HMS engagement, which do not need external ASIC. We’re working on the demo for this. If you’re interested, we can provide more details later.



Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,512件の閲覧回数
donikuy
Contributor III

Hi Lunmin,

I would also be interested in the HMS Profinet solution.

Could you please provide me with some information?

Kind Regards,

Ylber Doniku

0 件の賞賛
返信