Hello, everyone.
I did connect to P4080 through minicom for uploading RCW, u-boot, Kernel, Ramdisk image.
When the ramdisk image copy process had been completed, minicom wasn't interacting suddenly.
So I tried to quit and re-execute a minicom but it is not interacting like attached image file.
Please help me.
How could I re-connect to P4080 through minicom?
If the fully-reset solution for P4080 exists?
Thank you.
Okay, I will try the approach you said.
Thank you for persistently contributing to me.
I didn't know that I need CodeWarrior TAP.
No, I don't have. If I don't have CodeWarrior TAP, I couldn't solve this problem?
Thank you.
But I haven't an experience for CodeWarrior Flash Programmer so that may be hard challenge for me.
Could you give me a manual or simple description to program pre-compiled NOR flash image using CodeWarrior?
In this case it is recommended to use CodeWarrior Flash Programmer to program pre-compiled NOR Flash image provided in the ISO "QorIQ Linux SDK v2.0 PPCE500MC IMAGE":