How do you enable the network interfaces on the TWR-LS1021A to be able to communicate with external devices so far I am only able to use the network on the loop back network. The board is currently running the default linux ramdisk image that it ships with.
已解决! 转到解答。
Did you try ifconfig?
ifconfig(8): configure network interface - Linux man page
What does it say when you invoke it with '-a' ?
Have a great day
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Did you try ifconfig?
ifconfig(8): configure network interface - Linux man page
What does it say when you invoke it with '-a' ?
Have a great day
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
yes i did i was able to get the network link up and running after I switched to eth1. The switch i was using did not support 1gb/s networking which is what eth0 is configured at on the board. Now I have no issues using the network. Thanks for the help.