How to configure ethernet on TWR-LS1021A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure ethernet on TWR-LS1021A

ソリューションへジャンプ
1,269件の閲覧回数
colincox
Contributor I


How do you enable the network interfaces on the TWR-LS1021A to be able to communicate with external devices so far I am only able to use the network on the loop back network. The board is currently running the default linux ramdisk image that it ships with.

タグ(1)
0 件の賞賛
返信
1 解決策
778件の閲覧回数
bpe
NXP Employee
NXP Employee

Did you try ifconfig?

ifconfig(8): configure network interface - Linux man page

What does it say when you invoke it with '-a' ?


Have a great day

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
779件の閲覧回数
bpe
NXP Employee
NXP Employee

Did you try ifconfig?

ifconfig(8): configure network interface - Linux man page

What does it say when you invoke it with '-a' ?


Have a great day

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
778件の閲覧回数
colincox
Contributor I

yes i did i was able to get the network link up and running after I switched to eth1. The switch i was using did not support 1gb/s networking which is what eth0 is configured at on the board. Now I have no issues using the network. Thanks for the help.

0 件の賞賛
返信