Hi,
I am planning to used T2080 processor in my board. I need to achieve three x4 PCIe & two x4 SATA by using SerDes1 & SerDes2.
As per the SerDes register details given in the Table 19-2. SerDes Lanes Assignments and Multiplexing in the T2080_T2081 Reference Manual RevC.1(refer attachment) the there are two different register for two SerDes such as SRDS_PRTCL_S1 & SRDS_PRTCL_S2.
How to achieve three x4 PCIe & two x4 SATA ?
Regards
Soumya
How to achieve three x4 PCIe & two x4 SATA ?
This configuration is not supported.
Please, refer to T2080 RM Table 19-1 SerDes Lanes Assignments and Multiplexing.
- two x1 SATA are available (no x4 SATA)
- three x4 PCIe configuration can't coexist with SATA.
Closest match is : two x4 PCIe, one x2 PCIe and two x1 SATA
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [6C,16]
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [A4,16]
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [96,16]
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [8A,16]
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [66,16]
[SRDS_PRTCL_S1,SRDS_PRTCL_S2] = [66,15]
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------