Failed to configure lx2160 as sgmii

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to configure lx2160 as sgmii

767 次查看
jianghong
Contributor I

hello,

I am trying lx2160ardb is configured as sgmii, it is not successful,

1.Using lsdk for "flexbuild_lsdk2004_update_290520(lx2160ardb_rev2)"

2.Device tree configuration(Such as the red box

jianghong_0-1625638209666.pngjianghong_1-1625638237767.png

3. System part (Under the MDIO bus, you can see that the driver has been loaded)

jianghong_2-1625638382055.pngjianghong_3-1625638424409.png

The driver of sgmii is tested successfully under uboot, and the file can be downloaded,Only the device tree is configured in the kernel. I don't know if this configuration is feasible. Please give me a suggestion.

Thank you

 

 

0 项奖励
回复
1 回复

757 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to LX2160ARDB board Specifications from https://www.nxp.com/design/qoriq-developer-resources/layerscape-lx2160a-reference-design-board:LX216...

there is no SGMII PHY on the target board, so it is impossible to configure the Ethernet port of LX2160ARDB as SGMII mode.

0 项奖励
回复