想确认下:
1.使用FRWY-LS1046A-AC单板的代码是否可以兼容DDR4(MT40A1G16RC-062E)芯片?如果兼容,DDR4是否有降频的可能?
2.如果不兼容,是否有DDR4(MT40A1G16RC-062E)时序配置的相关patch?
3.如果没有patch,确认下是否只修改参数ddr_raw_timing(路径:packages/firmware/atf/plat/nxp/soc-ls1046/ls1046afrwy/ddr_init.c)即可?
解決済! 解決策の投稿を見る。
Please use English for future communications in NXP Community.
1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.
3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.
Regards,
Bulat
@Bulat Karymov OK,thanks。
Please use English for future communications in NXP Community.
1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.
3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.
Regards,
Bulat