FRWY-LS1046A-AC DDR4配置咨询

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRWY-LS1046A-AC DDR4配置咨询

Jump to solution
1,622 Views
tian_shuliang
Contributor I

想确认下:

 

1.使用FRWY-LS1046A-AC单板的代码是否可以兼容DDR4(MT40A1G16RC-062E芯片?如果兼容,DDR4是否有降频的可能?

2.如果不兼容,是否有DDR4(MT40A1G16RC-062E)时序配置的相关patch?

3.如果没有patch,确认下是否只修改参数ddr_raw_timing(路径:packages/firmware/atf/plat/nxp/soc-ls1046/ls1046afrwy/ddr_init.c)即可?

0 Kudos
Reply
1 Solution
1,350 Views
Bulat
NXP Employee
NXP Employee

Please use English for future communications in NXP Community.

1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.

3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.

Regards,

Bulat

View solution in original post

0 Kudos
Reply
2 Replies
1,350 Views
tian_shuliang
Contributor I

@Bulat Karymov  OK,thanks。

0 Kudos
Reply
1,351 Views
Bulat
NXP Employee
NXP Employee

Please use English for future communications in NXP Community.

1,2. The LS1046A supports DDR4 only. So yes, it is compatible with DDR4 in general and with MT40A1G16RC-062E in particular.

3. Yes, you can modify ddr_raw_timing in accordance with the new memory parameters.

Regards,

Bulat

0 Kudos
Reply