Could any one please reply to my below issues.
1. I have LS1088A board. I want to connect NVM PCIe 3.0 x4.0 SSD card to LS1088a board. Could you please suggest me which card will fit to LS1088a board(Provided below link) for NVM PCIe x4 also which slot number(there are 3 PCIe slot) in the LS1088a.?
2. is the NVM PCIe 3.0 x 4.0 SSD card supported mPCIe slot in LS1088a board ?
below is the link for Samsung 960 evo NVM PCIe card planning to purchase for experiment , is it work in LS1088a board as well its will give NVM PCIe x4 speed after connecting to the LS1088a board?