CAAM support in LS1027/1028??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAAM support in LS1027/1028??

866件の閲覧回数
milan_joshi
Contributor I

Is CAAM is supported in LS1027/1028?

0 件の賞賛
返信
2 返答(返信)

779件の閲覧回数
milan_joshi
Contributor I

Hi ufedor,

Thanks for responding to this, it is helpful.  I understood that there is SEC5 in LS series which is somewhat different than the HAB/AHAB in case of i.MX family.

0 件の賞賛
返信

779件の閲覧回数
ufedor
NXP Employee
NXP Employee

CAAM = Cryptographic Acceleration and Assurance Module

Also know as SEC (security engine).

There is no public revision of the LS1028ASECRM yet.

The LS1028A SEC is based on the LS1043A SEC, so it is possible to use the LS1043ASECRM for initial familiarization.

https://www.nxp.com/webapp/Download?colCode=LS1043ASECRM 

Updates to CAAM for LS1028A above what’s found on LS1043A:
• Second DESA engine
• Second PKHA engine
• New features in ERA10 for AESA
• New features in ERA10 for PKHA

0 件の賞賛
返信