About booting the DSP side of bsc9131

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About booting the DSP side of bsc9131

1,299 Views
symsong
Contributor II


     Hi,

          I'm following the Using PSC9131RDB BSP,A step by step guide to boot the DSP side of 9131,but now I get some questions,the guide says like below,

          Required binary images are already part of rootfs. The release contains a test firmware that is used to verify IPC function. To load this firmware on DSP, execute following command on Linux shell prompt: $ /ipc/dsp_bt /dsp_images/ipc_913x_dbg_0.5.bin

          but in my 9131's linux OS,the dsp_bt is a file instead of a directory,

          root@bsc913x:/ipc# ls -l

          -rwxr-x---    1 root     root          8441 Jun  7  2013 app

          -rwx------    1 root     root          8621 Jan 28  2014 dsp_bt

          -rwxr-x---    1 root     root          8329 Jan 28  2014 dsp_recover

          -rwx------    1 root     root          7538 Jan 28  2014 dump_mem

          -rwx------    1 root     root         11779 Jan 28  2014 ipc_test

          -rwx------    1 root     root         11312 Jan 28  2014 ipc_test67

          -rw-r--r--    1 root     root            34 Feb 21  2013 mem_dump_cfg.txt

          and if I just excute the ipc_test in the ipc dir,the endless log appears:

          main loop #ret  0

          main loop #ret  0

          main loop #ret  0

          .....

          What's wrong with that?

0 Kudos
Reply
3 Replies

1,179 Views
michelle
NXP Pro Support
NXP Pro Support

Hi

So this seems to be a misinterpretation:  dsp_bt is a program which is used to load the DSP code and set it to run.  It's usage is typically:

dsp_bt <dsp binary image.bin>

the example is just showing the paths to find each part (the bootloader program and the dsp binary image)...

Once this is done you should run the ipc_test application as this will be the Linux side application that sends and receives IPC messages (which the DSP binary image should also do).

0 Kudos
Reply

1,179 Views
symsong
Contributor II

And what's more,if I excecute dsp_bt,the result is

===DSP boot Application===(1.1.02)==

Usage:

dsp_boot

but it seems like there is something wrong,just like the doc says,

Appearance of ‘DSP Booted up’ confirms successful completion of DSP firmware upload.

0 Kudos
Reply

1,179 Views
symsong
Contributor II

Thanks,so what should I do now to run the DSP side(which is the Linux side send and receives IPC messages to DPS side)?

0 Kudos
Reply