QorIQ Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ Knowledge Base

Labels

Discussions

Sort by:
This section is essentially created to help all QorIQ Processing Platform users ranging from customers to designers to help provide the best solution to the most frequently encountered questions and  some handy tips & tricks related to QorIQ Processing Platform products.                                                   Frequently Asked Questions (FAQ) Tips & Tricks QorIQ P1 Devices QorIQ P1 Devices QorIQ P2 Devices QorIQ P2 Devices QorIQ P3 Devices QorIQ P3 Devices QorIQ P4 Devices QorIQ P4 Devices QorIQ P5 Devices QorIQ P5 Devices Feel free to browse through the various product FAQs to get answers to most commonly encountered questions on topics like DDR3, Ethernet (eTSEC), Booting, USB, Hardware Spec/Reference Manual and more. Also browse through the tips & tricks to help you with your design. Drop a comment or two on how we can keep building these pages. Also, feel free to give your suggestions on what you feel should be added to the FAQs or to the FAQ section as a whole. We intend the NXP Community to grow while mutually helping each other and by reducing design times by providing hands-on solution to tricky problems and questions. QorIQ P1 Devices P1010/1014 FAQs P1010/P1014 DDR Specific FAQs P1010/P1014 Ethernet (eTSEC) Specific FAQs P1010/P1014 USB Specific FAQs P1020/P1011 FAQs P1020/P1011 Clocking Specific FAQs P1020/P1011 COP/JTAG Specific FAQs P1020/P1011 Ethernet (eTSEC) Specific FAQs P1020/P1011 Hardware Specifications/Reference Manual Specific FAQs P1020/P1011 IBIS Specific FAQs P1020/P1011 Local Bus Specific FAQs P1020/P1011 Memory Controller Specific FAQs P1020/P1011 Reset Configuration Specific FAQs P1020/P1011 SPI Specific FAQs P1021/P1012 FAQs P1021/P1012 eSPI/FLASH Specific FAQs P1021/P1012 Ethernet (eTSEC) Specific FAQs P1021/P1012 Memory Controller/DDR Specific FAQs P1022/P1013 FAQs P1022/P1013 Clocking Specific FAQs P1022/P1013 DDR Specific FAQs P1022/P1013 Hardware    Specifications/Reference Manual Specific FAQs P1022/P1013 PCIe Specific FAQs P1022/P1013 Power Management Specific FAQs P1023/P1017 FAQs P1023/P1017 Clocking Specific FAQs P1023/P1017 DDR Specific FAQs P1023/P1017 PCIe Specific FAQs P1024/P1015 FAQs P1024/P1015 Clocking Specific FAQs P1024/P1015 eSPI/FLASH Specific FAQs P1024/P1015 Ethernet Specific FAQs P1024/P1015 Reset Configuration Specific FAQs P1024/P1015 Software Tools - CodeWarrior Specific FAQs P1025/P1016 FAQs P1025/P1016 Clocking Specific FAQs P1025/P1016 DDR Specific FAQs P1025/P1016 Hardware Specifications/Reference Manual Specific FAQs P1025/P1016 QUICC Engine Specific FAQs [ top of page ] QorIQ P1 Devices - Tips & Tricks                                            Booting P1020/P1011 from On-Chip ROM (eSDHC or eSPI) Booting P1021/P1012 from On-Chip ROM (eSDHC or eSPI) Booting P1022/P1013 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P1020/P1011 Booting to Linux from an SD Card/MMC for P1021/P1012 Booting to Linux from an SD Card/MMC for P1022/P1013 Enabling SD Interface on P1010 Reference Design Board Enabling SD Interface on P1023 Reference Design Board Enabling SD Interface on P1024 Reference Design Board Enabling SD Interface on P1025 Reference Design Board Hardware and Design Layout/Guidelines for P1010 DDR3 SRAM Interfaces Hardware and Design Layout/Guidelines for P1023 DDR3 SRAM Interfaces Hardware and Design  Layout/Guidelines for P1024 DDR3 SRAM Interfaces Hardware and Design Layout/Guidelines for P1025 DDR3 SRAM Interfaces [ top of page ] QorIQ P2 Devices P2010/P2020 FAQs P2010/P2020 Clocking Specific FAQs P2010/P2020 DDR Specific FAQs P2010/P2020 eSDHC Specific FAQs P2040/P2041 FAQs P2040/P2041 Clocking Specific FAQs P2040/P2041 Ethernet Specific FAQs P2040/P2041 Local Bus Specific FAQs P2040/P2041 PCIe Specific FAQs P2040/P2041 Pre-Boot Loader/Boot Sequencer Specific FAQs P2040/P2041 USB Specific FAQs P2040/P2041Hardware Specifications/Reference Manual Specific FAQs [ top of page ] QorIQ P2 Devices - Tips & Tricks    Booting P2010 from On-Chip ROM (eSDHC or eSPI) Booting P2040/P2041 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P2010 Booting to Linux from an SD Card/MMC for P2040/P2041 Enabling SD Interface on P2020 Reference Design Board Hardware and Design Layout/Guidelines for P2020 DDR3 SRAM Interfaces [ top of page ] QorIQ P3 Devices P3041 FAQs P3041 DDR Specific FAQs P3041 Ethernet Specific FAQs P3041 Hardware Specifications/Reference Manual Specific FAQs P3041 USB Specific FAQs [ top of page ] QorIQ P3 Devices - Tips & Tricks Hardware and Design Layout/Guidelines for P3041 DDR3 SRAM Interfaces [ top of page ] QorIQ P4 Devices                   P4040 FAQs P4040 Clocking Specific FAQs P4040 eSPI/FLASH Specific FAQs P4040 Ethernet Specific FAQs P4040 Reset Configuration Specific FAQs P4040 Software Tools - CodeWarrior Specific FAQs P4080 FAQs P4080 DDR Specific FAQs P4080 Ethernet Specific FAQs P4080 Hardware Specifications/Reference Manual Specific FAQs P4080 USB Specific FAQs [ top of page ] QorIQ P4 Devices - Tip & Tricks Booting P4080 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P4080 Hardware and Design Layout/Guidelines for P4040 DDR3 SRAM Interfaces [ top of page ] QorIQ P5 Devices P5020/P5010 FAQs P5020/P5010 COP/JTAG Specific FAQs P5020/P5010 Device Ratings Specific FAQs P5020/P5010 Hardware Specifications/Reference Manual Specific FAQs [ top of page ] QorIQ P5 Devices - Tips & Tricks Booting P5010 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P5010 Hardware and Design Layout/Guidelines for P5020 DDR3 SRAM Interfaces [ top of page ]
View full article
T4160 Block Diagram
View full article
DPDMUX is a device like DPSW (Switch) which allows switching of packets within the DPAA2 blocks. This application adds DPDMUX support in DPDK, uses LS2088ARDB as an example platform for demonstrating the use case that traffic bifurcation between DPDK and Linux Kernel using DPDMUX on DPAA2 platform.
View full article
Simple example T4240QDS project that incorporates the Mentor Graphics Embedded Performance Library (MEPL) to add Altivec coding.
View full article
Note (11/25): FAEs slowly replying with FAQs. This section is essentially created to help all Freescale Layerscape users ranging from customers to designers to help provide the best solution to the most frequently encountered questions and  some handy tips & tricks related to Freescale QorIQ Processing Platform products.                        Frequently Asked Questions (FAQ) Tips & Tricks QorIQ LS1 Devices QorIQ LS1 Devices QorIQ LS2 Devices QorIQ LS2 Devices Feel free to browse through the various product FAQs to get answers to most commonly encountered questions on topics like DDR3, Ethernet (eTSEC), Booting, USB, Hardware Spec/Reference Manual and more. Also browse through the tips & tricks to help you with your design. Drop a comment or two on how we can keep building these pages. Also, feel free to give your suggestions on what you feel should be added to the FAQs or to the FAQ section as a whole. We intend the Freescale Community to grow while mutually helping each other and help reduce design times by providing hands-on solution to tricky problems and questions. QorIQ LS1 Devices LS1020A/LS1021A/LS1022A FAQs LS102x FAQs LS102MA/LS1024A FAQs LS102MA/LS1024A Specific FAQs LS1043A FAQs P1020/P1011 Clocking Specific FAQs P1020/P1011 COP/JTAG Specific FAQs P1020/P1011 Ethernet (eTSEC) Specific FAQs P1020/P1011 Hardware Specifications/Reference Manual Specific FAQs P1020/P1011 IBIS Specific FAQs P1020/P1011 Local Bus Specific FAQs P1020/P1011 Memory Controller Specific FAQs P1020/P1011 Reset Configuration Specific FAQs P1020/P1011 SPI Specific FAQs [ top of page ] QorIQ LS1 Devices - Tips & Tricks                Booting P1020/P1011 from On-Chip ROM (eSDHC or eSPI) Booting P1021/P1012 from On-Chip ROM (eSDHC or eSPI) Booting P1022/P1013 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P1020/P1011 Booting to Linux from an SD Card/MMC for P1021/P1012 Booting to Linux from an SD Card/MMC for P1022/P1013 Enabling SD Interface on P1010 Reference Design Board Enabling SD Interface on P1023 Reference Design Board Enabling SD Interface on P1024 Reference Design Board Enabling SD Interface on P1025 Reference Design Board Hardware and Design Layout/Guidelines for P1010 DDR3 SRAM Interfaces Hardware and Design Layout/Guidelines for P1023 DDR3 SRAM Interfaces Hardware and Design  Layout/Guidelines for P1024 DDR3 SRAM Interfaces Hardware and Design Layout/Guidelines for P1025 DDR3 SRAM Interfaces [ top of page ] QorIQ LS2 Devices LS2085A FAQs P2010/P2020 Clocking Specific FAQs P2010/P2020 DDR Specific FAQs P2010/P2020 eSDHC Specific FAQs QorIQ LS2 Devices - Tips & Tricks Booting P2010 from On-Chip ROM (eSDHC or eSPI) Booting P2040/P2041 from On-Chip ROM (eSDHC or eSPI) Booting to Linux from an SD Card/MMC for P2010 Booting to Linux from an SD Card/MMC for P2040/P2041 Enabling SD Interface on P2020 Reference Design Board Hardware and Design Layout/Guidelines for P2020 DDR3 SRAM Interfaces [ top of page ]
View full article
What IDE is recommended for programming the LS1020A/LS1021A/LS1022A? The LS1 series is optimized for CodeWarrior, whose latest version, for ARMv7 can be found at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-LS-ARM7&fsrch=1. What is the LS102xA product family's enablement schedule up to 2016? The launch calendar for the LS102xA family is shown in the figure below. Can one CodeWarrior license cover both LS102x QDS and TWR? The full CW product can be used with either the TWR or QDS board through the CW-TAP probe. Does CodeWarrior for LS1 support flash (NOR/NAND) programming? Yes, CodeWarrior supports both NOR and NAND programming for QDS and TWR. Over what power range is LS102x designed for? LS102x is designed for operation under 3W.  Its ability to yield over 5000 Coremarks at a frequency of up to 1GHz separates the LS102x family from competitors in delivering improved performance without increased power consumption. How fast does the LS102x family run? The LS102x family can run between 600 MHz and and 1 GHz. What endianness does LS102x follow? The LS1 is based on the ARMv7 architecture, which is natively little-endian.  However, ARMv7 supports big-endian using the CPC15 register.  More significantly, many LS1 peripherals, like Ethernet and integrated flash controller (IFC), follow big-endian.  Therefore, LS1 is really a mixed-endian system and one must be mindful of a peripheral's endianness when programming the LS1.
View full article
IPSec Performance Reproducibility Procedure on T1040RDB platform 1. Enable ASF in Linux Kernel           Step 1: Launch the kernel menu using the command: bitbake -c menuconfig virtual/kernel      Step 2: Enable ASF under Device Driver -> Networking device support -> Application Specific Fastpath      Step 3: Build the final binaries that needs to be loaded on T1040RDB using the command : bitbake fsl-image-core NOTE: The ASF modules are compiled as dynamically loadable modules and placed in the ROOTFS under the path /usr/driver/asf/min and /usr/driver/asf/full 2. Steps to boot the board with 2 cores:  (optional) => cpu 2 disable => cpu 3 disable => boot Board configuration after Linux is up A. Enable ip_forwarding and Linux performance parameters echo 1 > /proc/sys/net/ipv4/ip_forward echo 9000 > /proc/sys/net/netfilter/nf_conntrack_udp_timeout echo 9000 >/proc/sys/net/netfilter/nf_conntrack_udp_timeout_stream B. Insmod ASF ko’s cd /usr/driver/asf/min insmod asf.ko insmod asfctrl.ko insmod asfipsec.ko insmod asfctrl_ipsec.ko C. Run fmc command : cd /usr/driver/asf/scripts/fmc/ fmc -s Soft_FragParser.xml -p asf-fman-perf-policy.xml -c asf-cfg-perf-2041.xml -a D. Assign interface IP addresses and routes according to setup. Left DUT: ifconfig fm1-gb0 172.18.18.10 netmask 255.255.0.0 up ifconfig fm1-gb3 200.200.200.10/24 up ifconfig fm1-gb1 172.20.20.10 netmask 255.255.0.0 up ifconfig fm1-gb4 20.20.20.10/24 up route add -net 192.168.1.0/24 gw 172.18.18.2 route add default gw 200.200.200.20 route add -net 172.168.1.0/24 gw 172.20.20.2 route add -net 172.168.2.0/24 gw 20.20.20.20 arp -s 172.18.18.2 00:00:00:00:00:01 (optional) arp -s 172.20.20.2 00:00:00:00:00:02 (optional) Right DUT: ifconfig fm1-gb0 172.19.19.10 netmask 255.255.0.0 up ifconfig fm1-gb3 200.200.200.20/24 up ifconfig fm1-gb1 172.21.21.10 netmask 255.255.0.0 up ifconfig fm1-gb4 20.20.20.20/24 up route add -net 192.168.2.0/24 gw 172.19.19.2 route add default gw 200.200.200.10 route add -net 172.168.2.0/24 gw 172.21.21.2 route add -net 172.168.1.0/24 gw 20.20.20.10 arp -s 172.19.19.2 00:00:00:00:00:02 (optional) arp -s 172.21.21.2 00:00:00:00:00:04 (optional) E. Configure IPSec policies and SAs (attached below that needs to be downloaded to the box via tftp or sftp) Left DUT: ./left_tun-4port-v1.txt Right DUT: ./right_tun-4port-v1.txt F. Switch settings killall -9 l2sw_bin l2sw_bin Using UIO: /dev/uio0 Mapped register memory @ 0xb7b3f000 Chipid: 099530e9 fsl_dpa ethernet.17 fm1-gb0: Err FD status = 0x00040000 fsl_dpa ethernet.18 fm1-gb1: Err FD status = 0x00040000 l2switch> l2switch>mac add 00:00:00:00:00:01 3 [MAC 00:00...00:01 is reachable on port 3] m2switch>mac add 00:00:00:00:00:03 7 l2switch>mac add 00:04:9f:03:30:f6 8 [MAC of fm1-gb0] l2switch>mac add 00:04:9f:03:30:f7 9 [MAC of fm1-gb1] l2switch>mac dump [Displays MACDB of switch (static & Dynamic)] Type VID MAC Address Ports ------ --- ----------------- ----- Static 1 00:00:00:00:00:01 3 Static 1 00:00:00:00:00:03 7 Static 1 00:04:9f:03:30:f6 8 Static 1 00:04:9f:03:30:f7 9 Static entries: 4 Dynamic entries: 0 l2switch> l2switch>^Z [Press ctrl+z to stop the process] [1]+ Stopped(SIGTSTP) l2sw_bin root@t1040rdb:/mnt/sridhar/asf-bins/qos/bin/full# killall -9 l2sw_bin G. Configure IXIA/STC to generate the traffic with 128 flows. H. Start the traffic from both end and verify all the flows are offloaded and packet is going through IPSec ASF. Note: Except switch settings everything is similar to previous performance releases by IDC. I. The ASF flow can be observed using the following command cat /proc/asf/flow_debug Script files PFA in attachment
View full article
Here is the vlan set up folw on P1010RDB.
View full article
More and more customers are using the Freescale Linux SDK/BSP for customized development, however, some use a stable but old kernel version. This is different from the Freescale publicly released SDK. In order to manage the gap and help apply the Freescale SDK/BSP more efficiently, Freescale provides backported Linux SDK/BSP according to the customer's kernel version requirements. This lecture summarizes the strategy and key technology of the backport, introduces the latest proactive backport model based on git release and will help expedite product development using Freescale Linux releases.
View full article
This document explains how to burn into target flash the binary files needed to boot the target board with u-boot and/or Linux from a released Digital Networking SDK. Start by identifying the SDK from which to extract the u-boot and Linux binaries.  SDK (and other BSP) files are archived here: http://linux.freescale.net/labDownload2/viewDownloads.php Enter "SDK" as your Filter Text to see only the SDK files. Pick the SDK that you want, and note the .iso files with -IMAGE- in the filenames, organized by processor cores.  For example, T4240 uses the e6500 core, so the IMAGE file with 64-bit binaries from SDK 1.7 would be QorIQ-SDK-V1.7-PPC64E6500-IMAGE-20141218-yocto.iso.  T1040 would use QorIQ-SDK-V1.7-PPCE5500-IMAGE-20141218-yocto.iso for 32-bit binaries, P1010 would use QorIQ-SDK-V1.7-PPCE500V2-IMAGE-20141218-yocto.iso, and so on.  Click on the -IMAGE- file you want and open it as a WinZIP file. The contents of each -IMAGE- .iso file are organized by specific target boards, so expand the WinZIP folder for the board you're using and you'll see the full list of all the files generated by that SDK for your board.  For example, 1.7 SDK for P2020-RDB (E500V2) would look like this: Next, refer to the Infocenter Boards page for details on what files need to go where. Expand the link for your board and click on the Flash Bank Usage link for the board you're using for board-specific details. Finally, refer to the Infocenter's System Recovery chapter for instructions on how to do the flash programming.  The two methods described are: use u-boot to download and program each file; or use the CodeWarrior Flash Programmer to do the same.  Both methods work, so use whichever method is easier. ALTERNATIVE: If you want a fully-loaded Linux system on your target board but you'd rather not have to individually flash a half-dozen files (while perhaps getting one or more of them wrong), most boards have complete, composite binary files in their -IMAGE- .iso archives.  Look in your mounted .iso file for the flash-image folder and you should see a list of files that look similar to this: Each of these _NOR_Flash.bin files includes everything from the RCW to the Linux kernel for the boards noted in their file names.  Program each file to the beginning address of the noted flash type (NAND, NOR, etc.) For example, on T4240-QDS, the beginning address of NOR is 0xE8000000, so program QorIQ_SDK_V1.7_T4240QDS-64B_20141218_NOR_Flash.bin to 0xE8000000. The advantage of this method is that you don't have to program multiple binary files, perhaps picking the wrong file or programming it to the wrong address.  The primary disadvantage is that this method takes a looooooong time since these _Flash.bin files are so large.  Also, you don't get to customize the configuration until after the file has been flashed and the board is up and running.
View full article
Here is the NAT set up flow on P1010RDB.
View full article
Recently I was handling a problem of E500 Data Cache flush. I have a study on this. Below is a summary/record of the study, here to post it for someone who may be interested in. 1. L1 D-Cache Flushing About Data Cache flush, there’s some description in E500 reference manual as below: Any modified entries in the data cache can be copied back to memory (flushed) by using a dcbf instruction or by executing a series of 12 uniquely addressed load or dcbz instructions to each of the 128 sets. The address space should not be shared with any other process to prevent snoop hit invalidations during the flushing routine. Exceptions should be disabled during this time so that the PLRU algorithm is not disturbed. The following methods can be used to flush a region in the L1 cache: • Perform reads to any 48-Kbyte region, then execute dcbf instructions to that region. Note that a 48-Kbyte region must be used to ensure that the PLRU algorithm flushes all of the cache entries (12 x 128 sets x 32 bits = 48 Kbytes). • Perform reads from any 48-Kbyte region that is guaranteed to not be modified in the L1 cache (for example, a ROM region). • Execute dcbz instructions to any 48-Kbyte scratch section, then invalidate the cache. Note that it is necessary to use a scratch region because some zeroed lines will be cast out. … On the e500v2 the HID0 register contains a field, DCFA (data cache flush assist), that, when set, forces the data cache to ignore invalid sets on miss replacement selection and follow the replacement sequence defined by the PLRU bits. This reduces the series of uniquely addressed load or dcbz instructions to eight per set. The bit should be set just before beginning a cache flush routine and should be cleared when the series of instructions is complete. 2. The Questions As the Data Cache size is 32 Kbytes, why 48 Kbytes region needs to be performed on? The manual uses an equation “12 x 128 sets x 32 bytes = 48 Kbytes” (here I assume it should be 32 bytes instead of 32 bits), it says a series of 12 uniquely addressed load to each of the 128 sets, but there is no explanation why it’s 12, and why uniquely? And more, it mentions the HID0 register filed DCFA. It says setting this field reduces the series of uniquely addressed load to eight per set. Why? This time there are more words “forces the data cache to ignore invalid sets on miss replacement selection and follow the replacement sequence defined by the PLRU bits”, how to understand? 3. Data Cache Basics To answer the questions above, we need to focus on the miss replacement selection algorithm as it refers to. But before this we should be clear about the Data Cache organization first, and know the “invalid sets” status. The E500 reference manual use below figure to describe the L1 D-Cache organization From this figure, we get 128 sets, 8 ways per set, and 32 bytes per way, which is 128 x 8 x 32 = 32 Kbytes. Here a block, also called a line/way, contains 8 words, or 32 bytes. Where a piece of data in memory should be placed into D-Cache? In other words what’s the mapping method between memory and the Cache? Each block is loaded from 8-words boundary, i.e. physical address bits PA[27:31] are zeros. Byte within a block is located by PA[27:31]. The set is selected by physical address bits PA[20:26], totally 2 7 =128, there is one set for each PA[20:26], or we say it’s one to one mapping. The tags consist of physical address bit PA[0:19], there are totally 2 20 kinds of tags but there are only 8 ways in each set, it’s one to multiple mapping. So we need replacement algorithm, in e500 the PLRU (pseudo-least-recently-used) replacement algorithm is used. 4. Miss Replacement In the reference manual it says “This algorithm prioritizes the replacement of invalid entries over valid ones (starting with way 0). Otherwise, if all ways are valid, one is selected for replacement according to the PLRU bit encodings shown in Table 11-8.” This is where the difference happened. Let’s analyze the easy case first, if HID0 register filed DCFA is set, all the ways are treated the same, valid or invalid will be ignored, only PLRU take effect. Assume PLRU bits are all zeros, below table shows the order ways be selected: B0 B1 B2 B3 B4 B5 B6 Ways selected 0 0 0 0 0 0 0 L0 1 1 1 0 0 0 0 L4 0 1 1 0 0 1 0 L2 1 0 1 0 1 1 0 L6 0 0 0 0 1 1 1 L1 1 1 0 0 1 1 1 L5 0 1 1 0 1 0 1 L3 1 0 1 0 0 0 1 L7 After 8 replacements, all the 8 ways are selected. Change PLRU bits to other values it’s still 8 replacements, that’s way it reduce 12 uniquely addressed load to 8. Then why it’s 12 if DCFA field is not set? Assume way 0,1,2,3 are invalid and way 4,5,6,7 are valid, and PLRU bits are all zeros, we have again the table as below: B0 B1 B2 B3 B4 B5 B6 Ways selected 0 0 0 0 0 0 0 L0 1 1 0 1 0 0 0 L1 1 1 0 0 0 0 0 L2 1 0 0 0 1 0 0 L3 1 0 0 0 0 0 0 L4 0 0 1 0 0 1 0 L0 1 1 1 1 0 1 0 L6 0 1 0 1 0 1 1 L2 1 0 0 1 1 1 1 L5 0 0 1 1 1 0 1 L1 1 1 1 0 1 0 1 L7 After 11 replacements, all the 8 ways are selected. Assume way 0,1,2,3,6,7 are invalid and way 4,5 are valid, and PLRU B5 is zero, we have again the table as below: B0 B1 B2 B3 B4 B5 B6 Ways selected - - - - - 0 - L0 1 1 - 1 - 0 - L1 1 1 - 0 - 0 - L2 1 0 - 0 1 0 - L3 1 0 - 0 0 0 - L6 0 0 0 0 0 0 1 L7 0 0 0 0 0 0 0 L0 1 1 1 0 0 0 0 L4 0 1 1 0 0 1 0 L2 1 0 1 0 1 1 0 L6 0 0 0 0 1 1 1 L1 1 1 0 0 1 1 1 L5 After 12 replacements, all the 8 ways are selected. Here 12 is the maximum replacement number, any other case will finish all 8 ways selected within 12 replacements. There are Cache operation code examples in NCSW for e500, including L1 D-Cache flushing, as attached. Also the whole article in attached as individual document.
View full article
If you are using Freescale QorIQ networking processors, and struggling with complicated and heavy work to analyze your code, there is something that can help --- Freescale Scenarios tool. You can make things simpler, and work more efficiently, right now. This article provides a short tour of the tool and provides in section one a brief  introduction to this tool, section two installation - section three getting started guide - section four a simple example – and finally in section five instructions for where you can find more docs and information. Thanks to Ed Martinez for the great support to this article! Please download the article attached for details.
View full article
QorIQ is a important contributor to the Internet of Things with devices such as the LS1 Gateway.  Read more about the Internet of Things! Freescale Expands System Power Management Portfolio to Its QorIQ LS1 Processors for a Secure Internet of Things
View full article
SPDK (Storage Performance Development Kit) is an optimized storage reference architecture. It is initiated and developed by Intel. SPDK provides a set of tools and libraries for writing high performance, scalable, user-mode storage applications. It achieves high performance by moving all of the necessary drivers into userspace and operating in a polled mode, like DPDK.
View full article
NXP T1040 and T1020 SoC have an 8-port gigabit Ethernet switch integrated on the device. QorIQ SDK includes an L2 Switch user space driver and a small demo application that uses the API provided by the switch driver. The L2Switch demo application is useful to configure switch in T1040. Attached document include steps modify the source code and add command to access switch registers, read or write, in SDK1.9. Before doing this, SDK1.9 needs to be installed and useable.  In the SDK manual, there are description about how to install the SDK, how to prepare host environment and how to setup poky for specific target.
View full article
Open source software development tools for ARM processors
View full article
I recently tried to update U-boot on the PSC9131RDB and struggled for a while with the DIP switches on the board. I thought I'd write up a few pointers in case you try to attempt this yourself. DIP switches for the PSC9131RDB are described on Infocenter here: http://www.freescale.com/infocenter/topic/QORIQSDK/4227333.html A couple of points about the switches and jumpers worth considering: Make sure you read the solder mask on the board. The switches are numbered upside down from what you might expect. SW6[3:4] describe how the JTAG chain is setup on the board. The Starcore and Power cores can be chained in the same scan chain, or separated. If this is set to 11, a side effect is that the NAND flash is write protected. Input clock to the 9131 can either be 66Mhz or 100MHz. Images are built to a specific input clock, so make sure you are using an image for the clock your board is set to. Jumper J16 (near the SMA connectors) configured the input clock to the processor. If the jumper is on, the input clock is 66MHz. If it is off, it's 100MHz. The clock PLL ratios are multiples of the input clock. CCB clock = the input clock * a multipler. The core frequency = CCB clock * multiplier. All of the multiplers are located in the DIP switches and must be changed if you move from an image built for 66MHz to an image built for 100MHz. For example: For a 66MHz input clock, my CCB multiplier = 6:1, so my CCB clock = 400MHz. My core multiplier = 2:1, so my core frequency = 400MHz * 2 = 800MHz. If I were to just switch the input clock to 100MHz with these settings, I'd be running my CCB at 100*6 = 600MHz, and my core at 1.2GHz (which violates the processor's spec's!). Lastly, the board is built with both SPI and NAND flash. You can boot from either. It's either / or, and the images are built differently, so make sure you have the correct image for what you're attempting. If you happen to have an image burnt into both of the flash devices (SPI and NAND) you may select which to use at boot through SW4[ROM_LOC]. This can be set to 0b0110 for SPI, or 0b1001 for NAND.
View full article
This document introduces how to implement Ethernet flow control in DPDK by setting BMAN hardware and software portal depletion entry and exit thresholds. Hardware and Software Portal Depletion Threshold Registers   BMAN Pool hardware Threshold configuration in DPDK.   Pause Quanta Configuration in DPDK Flow control configuration Implementation in DPDK  
View full article