Programming the registers of p4080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming the registers of p4080

Jump to solution
2,479 Views
sumanthmushiger
Contributor III

Hello all, I am new to embedded world, I am  completing the half done proting FreeRTOS on P4080 (half done by someother person), my task is to build the vPortEnableInterrupts, vPortDisableInterrupts & write UART driver for it. I am able to access the SPRs by defining them in cpuregister.h file like this -

#define CDCSR0  696

#define HID0    1008

#define hid0    1008

#define srr1    27 ... etc etc..

and the I could easily load these registers using instruction set nemonics like for example

mtspr r5, srr1

But now to write the UART driver, how do I define its registers ?

in the reference manual they have given the description like this

17.5.1 UART1 receiver buffer register (DUARTx_URBR)

These registers contain the data received from the transmitter on the UART buses. In

FIFO mode, when read, they return the first byte received. For FIFO status information,

refer to the UDSR[RXRDY] description.

Except for the case when there is an overrun, URBR returns the data in the order it was

received from the transmitter.

Addresses:      DUART1_URBR1 is 11C000h base + 500h offset = 11C500h

                      DUART1_URBR2 is 11C000h base + 600h offset = 11C600h

and also where do I have define them?

Please provide me with P4080 UART driver with its supporting files. Or atleast an example script of how can I use these registers.

Since this is my 1st project on embedded systems. your help will greatly appreciated.

regards,

Sam

Labels (1)
1 Solution
1,967 Views
marius_grigoras
NXP Employee
NXP Employee

Hi Sam,

These DUART registers are memory mapped registers (i.e. are accessible via memory and are mapped through CCSRBAR base address). The default CCSRBAR address value at P4080 is 0xfe000000.

So, you can simply define these registers as:

#define DUARTA_BASE (0xfe11c500)

#define DUARTB_BASE (0xfe11c600)

More of this, you can find in CW for PA a full example for P4080DS Serial in next path: PA\PA_Support\Serial\P4080DS_eabi_serial

Regards,

Marius

View solution in original post

3 Replies
1,968 Views
marius_grigoras
NXP Employee
NXP Employee

Hi Sam,

These DUART registers are memory mapped registers (i.e. are accessible via memory and are mapped through CCSRBAR base address). The default CCSRBAR address value at P4080 is 0xfe000000.

So, you can simply define these registers as:

#define DUARTA_BASE (0xfe11c500)

#define DUARTB_BASE (0xfe11c600)

More of this, you can find in CW for PA a full example for P4080DS Serial in next path: PA\PA_Support\Serial\P4080DS_eabi_serial

Regards,

Marius

1,967 Views
sumanthmushiger
Contributor III

Thank you very much Marius.

0 Kudos
Reply
1,967 Views
sumanthmushiger
Contributor III

is it some thing like this ?

volatile UINT32 * DUART_URBR1 = (volatile UINT32 *)(0x11C500);    

volatile UINT32 * DUART_URBR2 = (volatile UINT32 *)(0x11C600);

0 Kudos
Reply