MPC823ERDB 256MB DDR Support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC823ERDB 256MB DDR Support.

3,119 Views
vidyasagartata
Contributor II

Dear All,

We have developed custom MPC8323ERDB board.

We have 256MBytes DDR-2 SDRAM (MT4764M16 - 8Megx16x8banks) on board, we are able to access (read/write) 128Mbytes in u-boot.

Need to configure 256MBytes in u-boot.

Please let me know what configuration is needed access 256Mbytes DDR-2 SDRAM in u-boot.

Thanks,

Vidya 

Labels (1)
0 Kudos
Reply
20 Replies

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

Thanks for your very good support.

Please let me know how to test 256MB SDRAM in linux kernel, which tool is required.

I configured 256MB DDR, there is no kernel crash and Ethernet ports failing.

mtest is passing up to 0xFFFF000.

Thanks,

Sagar

0 Kudos
Reply

2,385 Views
Bulat
NXP Employee
NXP Employee

I believe your last question is not directly related to the original question of this thread, it is rather general linux question than MPC8323's one. In such a case please create a new thread next time.

As far as I know linux kernel supports MEMTEST feature that can help.

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

Please find log below:

U-Boot 2014.07-00038-g659b6a2-dirty (Jun 19 2016 - 10:01:26)MPC83XX

Reset Status: Software Hard, External/Internal Soft, External/Internal Hard

CPU:   e300c2, MPC8321E, Rev: 1.1 at 333.333 MHz, CSB: 133.333 MHz

Board: Freescale MPC8323ERDB

I2C:   ready

DRAM:  256 MiB (DDR2, 32-bit, ECC off, 266.667 MHz)

Flash: 256 MiB

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   UEC1, UEC3

Hit any key to stop autoboot:  0

=>

=>

=>

=>

=>

=> md 0xe0000000 0x40

e0000000: e0000000 00000000 00000000 00000000    ................

e0000010: 00000000 00000000 00000000 00000000    ................

e0000020: 80000000 80000019 00000000 00000000    ................

e0000030: fc000000 80000010 f8000000 80000019    ................

e0000040: 00000000 00000000 00000000 00000000    ................

e0000050: 00000000 00000000 00000000 00000000    ................

e0000060: 00000000 00000016 00000000 00000000    ................

e0000070: 00000000 00000000 00000000 00000000    ................

e0000080: 00000000 00000000 00000000 00000000    ................

e0000090: 00000000 00000000 00000000 00000000    ................

e00000a0: 00000000 8000001b 00000000 00000000    ................

e00000b0: 00000000 00000000 00000000 00000000    ................

e00000c0: 00000000 00000000 00000000 00000000    ................

e00000d0: 00000000 00000000 00000000 00000000    ................

e00000e0: 00000000 00000000 00000000 00000000    ................

' - try 'help'

=> md 0xe0000000 0x40

e0000000: e0000000 00000000 00000000 00000000    ................

e0000010: 00000000 00000000 00000000 00000000    ................

e0000020: 80000000 80000019 00000000 00000000    ................

e0000030: fc000000 80000010 f8000000 80000019    ................

e0000040: 00000000 00000000 00000000 00000000    ................

e0000050: 00000000 00000000 00000000 00000000    ................

e0000060: 00000000 00000016 00000000 00000000    ................

e0000070: 00000000 00000000 00000000 00000000    ................

e0000080: 00000000 00000000 00000000 00000000    ................

e0000090: 00000000 00000000 00000000 00000000    ................

e00000a0: 00000000 8000001b 00000000 00000000    ................

e00000b0: 00000000 00000000 00000000 00000000    ................

e00000c0: 00000000 00000000 00000000 00000000    ................

e00000d0: 00000000 00000000 00000000 00000000    ................

e00000e0: 00000000 00000000 00000000 00000000    ................

e00000f0: 00000000 00000000 00000000 00000000    ................

=> md 0xe0002000 0x80

e0002000: 0000000f 00000000 00000000 00000000    ................

e0002010: 00000000 00000000 00000000 00000000    ................

e0002020: 00000000 00000000 00000000 00000000    ................

e0002030: 00000000 00000000 00000000 00000000    ................

e0002040: 00000000 00000000 00000000 00000000    ................

e0002050: 00000000 00000000 00000000 00000000    ................

e0002060: 00000000 00000000 00000000 00000000    ................

e0002070: 00000000 00000000 00000000 00000000    ................

e0002080: 80844102 00000000 00000000 00000000    ..A.............

e0002090: 00000000 00000000 00000000 00000000    ................

e00020a0: 00000000 00000000 00000000 00000000    ................

e00020b0: 00000000 00000000 00000000 00000000    ................

e00020c0: 00000000 00000000 00000000 00000000    ................

e00020d0: 00000000 00000000 00000000 00000000    ................

e00020e0: 00000000 00000000 00000000 00000000    ................

e00020f0: 00000000 00000000 00000000 00000000    ................

e0002100: 00000000 00220802 26256222 0f9028c7    ....."..&%b"..(.

e0002110: c3080000 00401000 44400232 8000c000    .....@..D@.2....

e0002120: 00000000 00c80064 00000000 00000000    .......d........

e0002130: 02000000 00000000 00000000 00000000    ................

e0002140: 00000000 00000000 00000000 00000000    ................

e0002150: 00000000 00000000 00000000 00000000    ................

e0002160: 00000000 00000000 00000000 00000000    ................

e0002170: 00000000 00000000 00000000 00000000    ................

e0002180: 00000000 00000000 00000000 00000000    ................

e0002190: 00000000 00000000 00000000 00000000    ................

e00021a0: 00000000 00000000 00000000 00000000    ................

e00021b0: 00000000 00000000 00000000 00000000    ................

e00021c0: 00000000 00000000 00000000 00000000    ................

e00021d0: 00000000 00000000 00000000 00000000    ................

e00021e0: 00000000 00000000 00000000 00000000    ................

e00021f0: 00000000 00000000 00000000 00000000    ................

=>

But still ping does not work.

mtest does not have issue.

> mtest 0xa000000 0xb000000 0x919191 1

Testing 0a000000 ... 0b000000:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

=> mtest 0xb000000 0xc000000 0x919191 1

Testing 0b000000 ... 0c000000:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

=> mtest 0xc000000 0xd000000 0x919191 1

Testing 0c000000 ... 0d000000:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

=> mtest 0xd000000 0xe000000 0x919191 1

Testing 0d000000 ... 0e000000:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

=> mtest 0xe000000 0xf000000 0x919191 1

Testing 0e000000 ... 0f000000:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

=> mtest 0xf000000 0xf000fff 0x919191 1

Testing 0f000000 ... 0f000fff:

Pattern 00919191  Writing...  Reading...Tested 1 iteration(s) with 0 errors.

But if i do mtest 0xf000fff 0xffffeee 0x919191 1

board is getting reset.

Thanks,

Sagar

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

1. Please take a look at my post dated 07.06.2016 and make required changes.

2. As I can see you set SDRAM refresh period to 1.5us. SDRAM requires it to be 7.8us. Any special reason?

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

Please find the header file for DDR below:

/*

* DDR Setup

*/

#define CONFIG_SYS_DDR_BASE    0x00000000    /* DDR is system memory */

#define CONFIG_SYS_SDRAM_BASE    CONFIG_SYS_DDR_BASE

#define CONFIG_SYS_DDR_SDRAM_BASE    CONFIG_SYS_DDR_BASE

#define CONFIG_SYS_DDRCDR        0x62000002

#undef CONFIG_SPD_EEPROM

#if defined(CONFIG_SPD_EEPROM)

/* Determine DDR configuration from I2C interface

*/

#define SPD_EEPROM_ADDRESS    0x51    /* DDR SODIMM */

#else

/* Manually set up DDR parameters

*/

/*#define CONFIG_SYS_DDR_SIZE    64 */    /* MB */

#define CONFIG_SYS_DDR_SIZE    256    /* MB */

/* #define CONFIG_SYS_DDR_CS0_CONFIG    (CSCONFIG_EN \

                | CSCONFIG_ROW_BIT_13 \

                | CSCONFIG_COL_BIT_9)   */

                /* 0x80010101 */

//#define CONFIG_SYS_DDR_CS0_CONFIG    0x80840102

#define CONFIG_SYS_DDR_CS0_CONFIG    0x80844102

#define CONFIG_SYS_DDR_TIMING_0    ((0 << TIMING_CFG0_RWT_SHIFT) \

                | (0 << TIMING_CFG0_WRT_SHIFT) \

                | (0 << TIMING_CFG0_RRT_SHIFT) \

                | (0 << TIMING_CFG0_WWT_SHIFT) \

                | (2 << TIMING_CFG0_ACT_PD_EXIT_SHIFT) \

                | (2 << TIMING_CFG0_PRE_PD_EXIT_SHIFT) \

                | (8 << TIMING_CFG0_ODT_PD_EXIT_SHIFT) \

                | (2 << TIMING_CFG0_MRS_CYC_SHIFT))

                /* 0x00220802 */

/*#define CONFIG_SYS_DDR_TIMING_1    ((2 << TIMING_CFG1_PRETOACT_SHIFT) \

                | (6 << TIMING_CFG1_ACTTOPRE_SHIFT) \

                | (2 << TIMING_CFG1_ACTTORW_SHIFT) \

                | (5 << TIMING_CFG1_CASLAT_SHIFT) \

                | (3 << TIMING_CFG1_REFREC_SHIFT) \

                | (2 << TIMING_CFG1_WRREC_SHIFT) \

                | (2 << TIMING_CFG1_ACTTOACT_SHIFT) \

                | (2 << TIMING_CFG1_WRTORD_SHIFT))  */

                /* 0x26253222 */

//#define CONFIG_SYS_DDR_TIMING_1        0x3935d342

#define CONFIG_SYS_DDR_TIMING_1        0x26256222

#define CONFIG_SYS_DDR_TIMING_2     0x0f9028c7

/*

#define CONFIG_SYS_DDR_TIMING_2    ((1 << TIMING_CFG2_ADD_LAT_SHIFT) \

                | (31 << TIMING_CFG2_CPO_SHIFT) \

                | (2 << TIMING_CFG2_WR_LAT_DELAY_SHIFT) \

                | (2 << TIMING_CFG2_RD_TO_PRE_SHIFT) \

                | (2 << TIMING_CFG2_WR_DATA_DELAY_SHIFT) \

                | (3 << TIMING_CFG2_CKE_PLS_SHIFT) \

                | (7 << TIMING_CFG2_FOUR_ACT_SHIFT)) */

                /* 0x1f9048c7 */

#define CONFIG_SYS_DDR_TIMING_3    0x00000000

#define CONFIG_SYS_DDR_CLK_CNTL    DDR_SDRAM_CLK_CNTL_CLK_ADJUST_05

                /* 0x02000000 */

/*#define CONFIG_SYS_DDR_MODE    ((0x4448 << SDRAM_MODE_ESD_SHIFT) \ */

#define CONFIG_SYS_DDR_MODE    ((0x4440 << SDRAM_MODE_ESD_SHIFT) \

                | (0x0232 << SDRAM_MODE_SD_SHIFT))

                /* 0x44480232 */

#define CONFIG_SYS_DDR_MODE2    0x8000c000

/* #define CONFIG_SYS_DDR_INTERVAL    ((800 << SDRAM_INTERVAL_REFINT_SHIFT) \ */

#define CONFIG_SYS_DDR_INTERVAL    ((0x00c8 << SDRAM_INTERVAL_REFINT_SHIFT) \

                | (0x0064 << SDRAM_INTERVAL_BSTOPRE_SHIFT))

                /* 0x03200064 */

/*#define CONFIG_SYS_DDR_CS0_BNDS    0x00000003 */

//#define CONFIG_SYS_DDR_CS0_BNDS        0x00000007

#define CONFIG_SYS_DDR_CS0_BNDS        0x0000000F

#define CONFIG_SYS_DDR_SDRAM_CFG    0x43080000

/*#define CONFIG_SYS_DDR_SDRAM_CFG    (SDRAM_CFG_SREN \

                | SDRAM_CFG_SDRAM_TYPE_DDR2 \

                | SDRAM_CFG_32_BE) */

                /* 0x43080000 */

#define CONFIG_SYS_DDR_SDRAM_CFG2    0x00401000

#endif

/*

* Memory test

*/

#undef CONFIG_SYS_DRAM_TEST        /* memory test, takes time */

#define CONFIG_SYS_MEMTEST_START    0x00030000    /* memtest region */

//#define CONFIG_SYS_MEMTEST_END        0x03f00000

#define CONFIG_SYS_MEMTEST_END        0x07f00000

/*

* The reserved memory

*/

#define CONFIG_SYS_MONITOR_BASE    CONFIG_SYS_TEXT_BASE    /* start of monitor */

#if (CONFIG_SYS_MONITOR_BASE < CONFIG_SYS_FLASH_BASE)

#define CONFIG_SYS_RAMBOOT

#else

#undef  CONFIG_SYS_RAMBOOT

#endif

/* CONFIG_SYS_MONITOR_LEN must be a multiple of CONFIG_ENV_SECT_SIZE */

//#define CONFIG_SYS_MONITOR_LEN    (384 * 1024)    /* Reserve 384 kB for Mon */

#define CONFIG_SYS_MONITOR_LEN    (256 * 1024)    /* Reserve 384 kB for Mon */

#define CONFIG_SYS_MALLOC_LEN    (128 * 1024)    /* Reserved for malloc */

/*

* Initial RAM Base Address Setup

*/

#define CONFIG_SYS_INIT_RAM_LOCK    1

#define CONFIG_SYS_INIT_RAM_ADDR    0xE6000000 /* Initial RAM address */

#define CONFIG_SYS_INIT_RAM_SIZE    0x1000 /* Size of used area in RAM */

#define CONFIG_SYS_GBL_DATA_OFFSET    \

            (CONFIG_SYS_INIT_RAM_SIZE - GENERATED_GBL_DATA_SIZE)

/*

* Local Bus Configuration & Clock Setup

*/

#define CONFIG_SYS_LCRR_DBYP        LCRR_DBYP

#define CONFIG_SYS_LCRR_CLKDIV        LCRR_CLKDIV_2

#define CONFIG_SYS_LBC_LBCR        0x00000000

/*

* FLASH on the Local Bus

*/

#define CONFIG_SYS_FLASH_CFI        /* use the Common Flash Interface */

#define CONFIG_FLASH_CFI_DRIVER    /* use the CFI driver */

//#define CONFIG_SYS_FLASH_BASE    0xFE000000    /* FLASH base address */

#define CONFIG_SYS_FLASH_BASE        CONFIG_SYS_TEXT_BASE    /* FLASH base address */

//#define CONFIG_SYS_FLASH_SIZE        16    /* FLASH size is 16M */

#define CONFIG_SYS_FLASH_SIZE        64    /* FLASH size is 16M */

//#define CONFIG_SYS_FLASH_PROTECTION    1    /* Use h/w Flash protection. */

                    /* Window base at flash base */

#define CONFIG_SYS_LBLAWBAR0_PRELIM    CONFIG_SYS_FLASH_BASE

//#define CONFIG_SYS_LBLAWAR0_PRELIM    (LBLAWAR_EN | LBLAWAR_32MB)

#define CONFIG_SYS_LBLAWAR0_PRELIM    0x80000019

#define CONFIG_SYS_BR0_PRELIM    (CONFIG_SYS_FLASH_BASE \

                | BR_PS_16    /* 16 bit port */ \

                | BR_V)        /* valid */

#define CONFIG_SYS_OR0_PRELIM    0xFC000FF7

/*#define CONFIG_SYS_OR0_PRELIM    (MEG_TO_AM(CONFIG_SYS_FLASH_SIZE) \

                | OR_GPCM_XAM \

                | OR_GPCM_CSNT \

                | OR_GPCM_ACS_DIV2 \

                | OR_GPCM_XACS \

                | OR_GPCM_SCY_15 \

                | OR_GPCM_TRLX_SET \

                | OR_GPCM_EHTR_SET \

                | OR_GPCM_EAD) */

                /* 0xFE006FF7 */

#define CONFIG_SYS_MAX_FLASH_BANKS    2    /* number of banks */

//#define CONFIG_SYS_MAX_FLASH_SECT    128    /* sectors per device */

#define CONFIG_SYS_MAX_FLASH_SECT    1024    /* sectors per device */

#undef CONFIG_SYS_FLASH_CHECKSUM

/* Second Flash */

#define CONFIG_FLASH1_BASE    0x88000000

#define CONFIG_LBLAWBAR1_PRELIM    CONFIG_FLASH1_BASE

#define CONFIG_LBLAWAR1_PRELIM             0x80000019 /*LBLAWAR2  - enable, size = 64MB */

#define CONFIG_SYS_BR1_PRELIM  (CONFIG_FLASH1_BASE |      /* Flash Base address */ \

                        (2 << BR_PS_SHIFT) |    /* 16 bit port size */ \

                        BR_V)                   /* valid */

#define CONFIG_SYS_OR1_PRELIM          0xFC000FF7      /* Mask for 64MB Flash size */

/*

* Memory map for DS0 Cross Connect

*/

#define CONFIG_SYS_LBLAWBAR2_PRELIM    0xFC000000

#define CONFIG_SYS_LBLAWAR2_PRELIM             0x80000010 /*LBLAWAR2  - enable, size = 128KB*/

//#define CONFIG_SYS_LBLAWAR2_PRELIM           0x80000011 /*LBLAWAR2  - enable, size = 256KB*/

#define CONFIG_SYS_BR2_PRELIM 0xFC001001 /* BR2 base address at 0xFA008000, port size 16 bit, */

#define CONFIG_SYS_OR2_PRELIM 0xFFFE0FF7 /* OR2 128KB size */

//#define CONFIG_SYS_OR2_PRELIM 0xFFFC0FF7 /* OR2 256KB size */

Please find the DDR section:

DDR_8323ERDB.jpg

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

1. Please take a look at my post dated 07.06.2016 and make required changes.

2. Your schematics is not well visible due to low resolution.

After changes are made, please take following memory dumps in uboot:

md e0000000 40

md e0002000 80

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

I have chenged

#define CONFIG_SYS_DDR_CS0_CONFIG    0x80840102

#define CONFIG_SYS_DDR_TIMINING_2            0x0f9030c7

and tested DDR2 SDRM but result is same.

Please suggest me what is the issue.

Thanks,

Sagar 

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

I have changed the macros

#define CONFIG_SYS_CS0_CONFIG 0x80844102

#define CONFIG_SYS__DDR_TIMING_2      0xf9028c7

But still ping does not happen.

Thanks,

Vidya

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

Can you attach actual header file (for 256MB) and actual schematics of the DDR interface?

Regards,

Bulat

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

Again, header file seems to be old. Another example from the file:

#define CONFIG_SYS_DDR_CS0_CONFIG    0x80840102

This value corresponds to 128MB memory size.

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

If i changed the value of

#define CONFIG_SYS_DDR_TIMINING_2                0x0f9030c7

and cross ported compiled u-boot but is same, Ethernet ports are not working.

Thanks,

Sagar

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

As I can see you sent old header file, values of DDR controller do not correspond to mentioned above. For example:

#define CONFIG_SYS_DDR_TIMING_2     0x0f9030c7

You mentioned:

#define CONFIG_SYS_DDR_TIMING_2 0x0f9028c7                    //old =0x0f9030c7

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

I have changed but facing same problem.

I have attached the MPC8323ERDB.h config file.

Please help me to solve the issue.

Thanks,

Sagar

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

There is no problem in the 128MBytes read and write and in this case both Ethernet ports work.

But when enabled the 256MBytes DDR SRAM,in this case both Ethernet port do not work.

Whenever ping, gets hang.

MCK ferquency on the DDR bus = 133.33 MHz.

Thanks,

Sagar

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

Following line is not correct for 133MHz, DDR2 fucntionality will be corrupted:

#define CONFIG_SYS_DDR_TIMING_1 0x26256222               //old = 0x3935d342

It needs to be like following:

#define CONFIG_SYS_DDR_TIMING_1 0x2625A222        

Also we recommend that WL+AL should be a minimum of 3 cycles for the ODT to be asserted correctly. In your case AL=0, so this recommendation is not met.

Regards,

Bulat

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

Can you clarify if something has changed after your original question? You wrote "we are able to access (read/write) 128Mbytes in u-boot", is it still so? You did not mention the word "ethernet" in the first question.

What is the MCK frequency on the DDR bus?

Regards,

Bulat

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Dear Bulat,

You are correct

#define CONFIG_SYS_DDR_SYS                256                        // MB

#define CONFIG_SYS_CS0_CONFIG          0x80844102          // old = 80840102

#define CONFIG_SYS_IBAT0L                    (CONFIG_SYS_SDRAM_BASE | BATU_BL_256M | BATU_VS | BATU_VP )

Also changed the timing parameters for accessing (read/write) 256 MBytes

#define CONFIG_SYS_DDR_TIMING_1 0x26256222               //old = 0x3935d342

#define CONFIG_SYS_DDR_TIMING_2 0x0f9028c7                    //old =0x0f9030c7

256MBytes detects in u-boot as well as in kernel also cat /proc/meminfo shows MemTotal:   255012 KB

but  Ethernet is not working in both u-boot and kenrnel and also getting restarted if i do ping.

Please let me know any more parameter need to change for accessing (read/write) 256MBytes DDR SDRAM memory.

Thanks,

Sagar

0 Kudos
Reply

2,387 Views
vidyasagartata
Contributor II

Hi Bulat,

I changed following parameters according to the 8323RM and DDR-2 data sheet,

DDR_CS0_CONFIG 256                                             // old = 64

DDR_CS0_BNDS 0x0000000F                                  // old = 0x00000003

128MBytes DDR SDRAM works fine at following configuration (include/configs/MPC8323ERDB.h)

DDR_CS0_CONFIG 128                                    // old = 64
DDR_CS0_BNDS 0x00000007                              // old = 0x00000003

MMU setup is always (Both cases)

CONFIG_HIGH_BATS            1

Please let me know any other value need to modified to access (read/write) 256MBytes DDR SDRAM.

Thanks,

Vidya

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

Following line is a bit doubtful:

DDR_CS0_CONFIG 256                                             // old = 64

Can you check it once again?

--------------------------------------------------------------------

1) I believe you were going to set :

#define CONFIG_SYS_DDR_SIZE    256    /* MB */

2) DDR_CS0_CONFIG should be 0x80014102 in your case.

3) Check that CONFIG_SYS_IBAT0U is set to BATU_BL_256M size.

Regards,

Bulat

0 Kudos
Reply

2,387 Views
Bulat
NXP Employee
NXP Employee

DDR SDRAM size should be properly set in three places:

1) DDR controller itself;

2) SDRAM local access window;

3) IBAT/DBAT MMU registers.

Try to check if all these settings are correct.

Regards,

Bulat

0 Kudos
Reply