Hi all!
I got a loaner from freescale as they sent ut a new board. This loaner is a b4860qds board. When I try to use tftp commands in u-boot to flash to the board, I get this:
Retry count exceeded; starting again
FM1@DTSEC5 Waiting for PHY auto negotiation to complete......... TIMEOUT !
FM1@DTSEC5: No link.
FM1@DTSEC6 Waiting for PHY auto negotiation to complete......... TIMEOUT !
FM1@DTSEC6: No link.
FM1@TGEC1: Tx buffer not ready
FM1@TGEC1: Tx buffer not ready
Using FM1@TGEC1 device
TFTP from server 10.10.1.42; our IP address is 10.10.65.24
Filename '/tftpboot/lahav-b4860qds-loaner/rcw_new.bin'.
Load address: 0x1000000
Loading: FM1@TGEC1: Tx buffer not ready
FM1@TGEC1: Tx buffer not ready
T FM1@TGEC1: Tx buffer not ready
Only the J20 ethernet port seems to work (green light), so I am using that one. All parameters are good as far as I can tell. Any ideas what might be going on?
Thanks!
Your IP address and IP address of your TFTP server is different. Test your board if the B4860QDS IP address is 10.101.24 or similar.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
Thanks for the reply. Yes, the IP address of the b4860qds s 10.10.65.24, the IP address of the server is 10.10.1.42, and the mask is 255.255.0.0. This exact configuration works well with another b4860qds board we have in the same subnet. So this cannot be because of the configuration. I believe there is a hardware problem with the ethernet device.
I think I will return the board to freescale.
Thanks!
Do you use the same netmask on your PC and your gateway?
Test your board using ping command from u-boot and ipaddr 10.10.1.xx.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------