Can anybody share the i2c2 user guide for the bsc9132qds?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can anybody share the i2c2 user guide for the bsc9132qds?

832 次查看
manjanagoudapat
Contributor III


wusdk has the user manual for i2c on the bsc9131rdb. but i need the i2c user manual for bsc9132qds as the i2c2 interface is complex.

thanks and regards

patil

标签 (1)
0 项奖励
回复
1 回复

700 次查看
Pavel
NXP Employee
NXP Employee

The BSC9132QDS driver is common I2C Linux driver.

Look at the following pages for I2C using under Linux:

https://xgoat.com/wp/2007/11/11/using-i2c-from-userspace-in-linux/

http://www.haifux.org/lectures/258/gpio_spi_i2c_userspace.pdf

https://www.kernel.org/doc/Documentation/i2c/dev-interface

http://elinux.org/Interfacing_with_I2C_Devices


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复