T4241 processor RESET_REQ_B signal probe output looks like continous pulses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4241 processor RESET_REQ_B signal probe output looks like continous pulses

Jump to solution
1,736 Views
kumar_086
Contributor IV

Dear Experts,

We are bringing up a T4241 processor board, loaded with RCW file in NOR Flash. In other boards we are able to see U-Boot booting.

In a particular board when we power on the board with UART, there is continuous character '' (triple bar) is printing on the terminal.

When we probed the processor signals its observed that signal 'RESET_REQ_B' output looks like a pulsed signal.

I'm new to this platform and requesting your help to resolve this.

Thanks

0 Kudos
Reply
1 Solution
1,714 Views
r8070z
NXP Employee
NXP Employee

It is supposed that RESET_REQ signal triggers circuit which assigns PORESET (or HRESET). On reset RESET_REQ is negated and device tried to start. So we can imagine that toggling RESET_REQ signal means that during start due to some error device assigns RESET_REQ and as result is trying to start again and again. Possible reasons for RESET_REQ_B assertion you can find in the section “Reset Request Status Register (DCFG_CCSR_RSTRQSR1)” of the QorIQ T4240 Reference Manual. Probably Uboot image in the NOR flash has been damaged and device executes something wrong.

View solution in original post

0 Kudos
Reply
2 Replies
1,361 Views
kumar_086
Contributor IV

Thanks r8070z. After reprogramming Uboot image once again in NOR Flash, it's working now.

Regards!

0 Kudos
Reply
1,715 Views
r8070z
NXP Employee
NXP Employee

It is supposed that RESET_REQ signal triggers circuit which assigns PORESET (or HRESET). On reset RESET_REQ is negated and device tried to start. So we can imagine that toggling RESET_REQ signal means that during start due to some error device assigns RESET_REQ and as result is trying to start again and again. Possible reasons for RESET_REQ_B assertion you can find in the section “Reset Request Status Register (DCFG_CCSR_RSTRQSR1)” of the QorIQ T4240 Reference Manual. Probably Uboot image in the NOR flash has been damaged and device executes something wrong.

0 Kudos
Reply