hello
I have compiled the uboot and linux kernel with LTIB ,than transplate the uboot and kernel (uImage) to the board(MPC8313ERDB). The uboot goes well ,print as follows:
Reset Status:
CPU: e300c3, MPC8313E, Rev: 21 at 333.333 MHz, CSB: 166 MHz
Board: Freescale MPC8313ERDB
I2C: ready
DRAM: 128 MB
FLASH: 8 MB
NAND:
In: serial
Out: serial
Err: serial
Net: TSEC0, TSEC1 [PRIME]
=>
than after transplant the uImage , reset and boot the board
=>bootm fe100000 fe300000 fe700000
print as follows:
## Booting image at fe100000 ...
Image Name: Linux-2.6.23
Created: 2013-03-29 3:22:25 UTC
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 1619970 Bytes = 1.5 MB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Uncompressing Kernel Image ...
It stops ! There must be something wrong , but why ?help me !
ps:Old uInage is OK for the boot !
Asky
已解决! 转到解答。
I've got the same problem...
so ,you 've just clean out your kernel config?
I got this message at the end of compiling the kernel
INFO: Uncompressed kernel (size 0x9f2000) overlaps the address of the wrapper(0x400000)
INFO: Fixing the link_address of wrapper to (0xa00000)
How can I increase the possible size?
thanks
Those messages are not relevant unless you're using the bootwrapper (e.g. cuImage), which you're not. Even then, the message just indicates that the addresses have been updated to compensate.
I think you may be seeing an old U-Boot bug involving speculative accesses to a mapping that should be marked guarded but isn't. U-Boot 1.3.0 is very old. Please use a current upstream version.