T1024 DDR VALIDATION PROBLEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 DDR VALIDATION PROBLEM

1,089件の閲覧回数
Jaygao
Contributor I

The development board based on T1024 uses 5 MT40A256M26LY-062E DDR4 chips. Below are the settings in DDRTOOL, as well as the verification results and logs. No matter how the DDR configuration is changed, the results are the same. in addition, the Relative delay time of between MCKE signal and ddr_RST is about 2S.would you like to inquire if there is a problem with the settings or provide some ideas to solve the problem? Thank you

 

0 件の賞賛
返信
0 返答(返信)