Mpc8548 Development Environment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Mpc8548 Development Environment

跳至解决方案
1,117 次查看
systick
Contributor II

Hi All, 

I find somewhere a board it has mcp8548 processor its PowerPC arch., now I want to install Linux on this board, I set the U-Boot, I have to install U-Boot to processor, boards has a jtag interface and I have multilink-fx development interface, here is the problem;

How can I set the development environment ? 

标记 (3)
0 项奖励
回复
1 解答
875 次查看
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
876 次查看
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复