MPC8309 pin mux tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,331件の閲覧回数
Sw2
Contributor I

Hi,

I am not able to download MPC8309 pin mux tool 'NetComme 4.2' from Design : Product Information : NetComm Software Resources (flexnetoperations.com)

I have received a mail stating that this software product has been added to my software account.

Still I am unable to download the file.

0 件の賞賛
返信
1 解決策
4,293件の閲覧回数
ufedor
NXP Employee
NXP Employee
0 件の賞賛
返信
14 返答(返信)
4,300件の閲覧回数
Sw2
Contributor I
0 件の賞賛
返信
4,294件の閲覧回数
ufedor
NXP Employee
NXP Employee
0 件の賞賛
返信
4,272件の閲覧回数
Sw2
Contributor I

Thanks. Now I am able download the files.

Is it a codewarrior plugin ?

Is there any CommExpert pin mux tool for MPC8309 like MPC8306?

 

0 件の賞賛
返信
4,268件の閲覧回数
ufedor
NXP Employee
NXP Employee

Have you installed CommExpert 4.2?

0 件の賞賛
返信
4,251件の閲覧回数
Sw2
Contributor I

Yes. I have installed CommExpert. But it is for mpc8306 not mpc8309

0 件の賞賛
返信
4,249件の閲覧回数
ufedor
NXP Employee
NXP Employee

What is the name of the downloaded file?

Please provide screenshot of the "About CommExpert" window.

0 件の賞賛
返信
4,186件の閲覧回数
Sw2
Contributor I

CommExpert.PNG

0 件の賞賛
返信
4,181件の閲覧回数
Sw2
Contributor I

Hi,

How we get CommExpert 4.2 ?

I could not find it.

0 件の賞賛
返信
4,145件の閲覧回数
mtom8735
Contributor I

Hi @ufedor ,

I was also not able to find the download link for CommExpert4.2 for MPC8309 board. Are there any available links ?


0 件の賞賛
返信
4,141件の閲覧回数
ufedor
NXP Employee
NXP Employee
0 件の賞賛
返信
4,035件の閲覧回数
mtom8735
Contributor I

Is the above suite (NetComm.jpg) to be used along with code warrior or eclipse for performing the pin muxing configuration. If so, are there any documents for reference.

0 件の賞賛
返信
4,029件の閲覧回数
ufedor
NXP Employee
NXP Employee

proprietary_netcomm_software_r4_2 is a standalone application.

0 件の賞賛
返信
4,005件の閲覧回数
mtom8735
Contributor I

I need to perform the configuration for MPC8309 for which I think proprietary_netcomm_software_r4_4 is required. But after installing proprietary_netcomm_software_r4_4 I could not find the standalone application.

proprietary_netcomm_software_r4_2 does not have the option for MPC8309. See attachment.
Would appreciate any help for configuring MPC8309 as I am new to this.

0 件の賞賛
返信
4,318件の閲覧回数
ufedor
NXP Employee
NXP Employee
0 件の賞賛
返信