MPC8308 Support for Non-OS based applications

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8308 Support for Non-OS based applications

跳至解决方案
1,985 次查看
venkateshn
Contributor II

Hi,

I am planning to use MPC8308 processor for Non OS (Firmware) based standalone applications, kindly let me know the suitability of this part.

Regards,

Venkatesh N

标签 (3)
0 项奖励
回复
1 解答
1,707 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, MPC8308 is suitable for standalone applications.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

6 回复数
1,707 次查看
venkateshn
Contributor II

Dear alexander.yakovlev,

can you suggest me the standalone application IDE and Compiler for MPC8308 processor.

Note: please share me the standalone example codes.

Regards,

Venkatesh N

0 项奖励
回复
1,707 次查看
alexander_yakov
NXP Employee
NXP Employee

We recommend using our CodeWarrior software for that purpose:

CodeWarrior Development Tools for PowerQUICC|Freescale

Please look default "Hello World" project in CodeWarrior for standalone project example code.

1,707 次查看
venkateshn
Contributor II

Hi,

I have installed CodeWarrior 8.8.5version. But i did not find any Hello World example for MPC8308 in installed CW folder.

Please share me the link or NON OS based examples to realize all interfaces related to Evaluation board (MPC8308RDB).

Thanks & Regards,

Venkatesh N

0 项奖励
回复
1,707 次查看
alexander_yakov
NXP Employee
NXP Employee

Please press "File" - "New", enter project name and location, and select "EPPC New Ptoject Wizard". On the next screen select Freescale linker, than on the next screen - MPC83xx tab, MPC8308 device and board you are using, than language type C or C++ and debug probe type. Finally, generated default project will be standalone application for bare board.

0 项奖励
回复
1,707 次查看
venkateshn
Contributor II

alexander.yakovlev

alexander.yakovlev i have purchased MPC8308-RDB Evaluation board for my application development but it is of OS based so can you share any MPC8308 Non OS based applications for my reference.

Regards,

Venkatesh N

0 项奖励
回复
1,708 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, MPC8308 is suitable for standalone applications.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------