How to test NVRAM in Yacto Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test NVRAM in Yacto Linux

Jump to solution
1,771 Views
vinothkumars
Senior Contributor IV

Hi All,

I am using Power PC and I want to test NVRAM.

1> Is it any commands to test nvram in command prompt ?

2> How to write, read and erase NVRAM ?

Regards,

VinothS

Regards,
Vinothkumar Sekar
Tags (2)
0 Kudos
Reply
1 Solution
1,386 Views
Pavel
NXP Employee
NXP Employee

Often u-boot is used for RAM test.

U-boot contains simple memory test.

See the following pages:

https://github.com/LeMaker/u-boot/blob/master/doc/README.memory-test

 

http://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,387 Views
Pavel
NXP Employee
NXP Employee

Often u-boot is used for RAM test.

U-boot contains simple memory test.

See the following pages:

https://github.com/LeMaker/u-boot/blob/master/doc/README.memory-test

 

http://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,386 Views
vinothkumars
Senior Contributor IV

Thank you Pavel, I closed this thread now.

Regards,
Vinothkumar Sekar
0 Kudos
Reply