Hello,
The board is LS1046 FRWY. The CWTAP I have is as below links. The COM port of CWTAP is visible from the device manager and its netparam can be checked as below picture. However, the connection is not found from CW connections view. How to debug this issue?
CWH-CTP-BASE-HE NXP Semiconductors | Mouser Taiwan
CWH-CTP-CTX10-YE NXP Semiconductors | Mouser Taiwan
Thanks.
Attach one more video to display connections view.
Please note, the IP address is my CW ethernet address, please add customer's own CW IP address.
It seems before, you connect the CW through ethernet.
Please set the IP address in the probe type space.
See attachment.
Or link the CW with USB cable.
Would you PC could ping CWTAP?
Would you connect the USB cable first?
Have you try to connect the USB cable first? Not the ethernet?
What's the CW version? Is it 11.5.12?
Have you tried to create a new project in a brand-new file?
If it's not work, would try to re-install the CW, try it on a new PC
June, As you can see from the previously attached picture, the project name is "NEW PROJECT". It is a newly created project. The CW version you mentioned is correct.
Have you tried to create a new project in a new workspace(a brand-new file)?
Please create a new project in the QCVS windows, you would see the "Connections View" in the QCVS windows.
But, if you want to check the board link. It seems you have duplicated a new board. Press the "Diagnose Connections"
Window > Perspective > Open Perspective> Others>Target Connections>C/C++(default)>Target Connections.