Wake-up from KL15 with IO_O pin and again to enter to sleep or different mode on FS6500 series SBC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wake-up from KL15 with IO_O pin and again to enter to sleep or different mode on FS6500 series SBC

2,012 Views
alicanozpay
Contributor II

Hello, 

I am using FS6500 series SBC on safe mode. When I give signal from IO_O wake pin, my system can be awake but after 1-2 second automaticaly goes to down. Maybe go to LPOFF modes.

How can ı take diagnostic where ı am make wrong configuration or where is the mistake? 

My configuration are listed below.

Select resistor is 24 k and connected to GND.

FS0B pin connected to MCU with pulled up by 10K to VSUP3

  • There is ignition input on IO_O.
  • VKAM did not connect to MCU.
  • FCCU_F1 connected to MCU with pulled up by 5.1K to VDDIO.
  • FCCU_F0 connected to MCU with pulled down by 10K to GND.
  • SPI communication connected to MCU.
  • RSTB connected to MCU with pulled up by 5.1K to VDDIO.
  • I am using buck-boost configuration with external mosfet.

I am thinking the SBC can go to WAKE-UP phase on main state machine but after 1- 2second go to LPOFF mode a thing happened.

Maybe this issue about watchdog timer.. I don't know.

*Note : I can see the required all voltage level when ı give signal from IO_O in a period of 1-2 second.

Best regards,

Alican OZPAY

R&D Engineer

0 Kudos
Reply
3 Replies

1,986 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can attached here,if it's confidential please submit a case we will review it!

Home (nxp.com)

0 Kudos
Reply

2,003 Views
guoweisun
NXP TechSupport
NXP TechSupport

1: share with your schematic

2:except wakeup issue,any other issue be found?

0 Kudos
Reply

1,997 Views
Aozpay
Contributor II

Could you please give e-mail to me for sharing?

0 Kudos
Reply