VR5510 Bandgap voltage specification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VR5510 Bandgap voltage specification

跳至解决方案
1,797 次查看
K_Steinhammer
Contributor III

In an application with functional safety requirements, we need an independent reference voltage for periodically testing the ADC of the CPU.

Now there is the idea to measure one bandgap voltage of the VR5510 PMIC via the AMUX pin for reference. Unfortunately the bandgap voltage specifications are missing in the datasheet.

Is there a document with the missing specifications (voltage and accuracy of Bandgap Main and Bandgap Fail-safe)?

Thanks.

标签 (1)
标记 (1)
0 项奖励
1 解答
1,599 次查看
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

在原帖中查看解决方案

0 项奖励
3 回复数
1,600 次查看
K_Steinhammer
Contributor III

Maybe this information is not available to the public - I got an answer within 24h after opening a support ticket (I have an active NDA).

So I advice anybody needing this information to do the same.

Thanks

0 项奖励
1,784 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below :

1: customer name/location

2: end product/

3:schedule

4: volume/annual

0 项奖励
1,774 次查看
K_Steinhammer
Contributor III

Requested information is sent via a PM.

 

Thanks

0 项奖励