The problem with using UJA1164 (S32K118 is used for MCU)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem with using UJA1164 (S32K118 is used for MCU)

521 Views
Caleb1
Contributor I

When using UJA1164, opening the watchdog will cause MCU reset when receiving CAN data? Is there a routine like this that can be provided?

When using UJA1164, the default time for opening the watchdog is 128ms. If the dog is fed within 97ms, what will be the impact? Will it reset regardless of sending or receiving CAN data?

When using UJA1164, the default time for opening the watchdog is 128ms, which has been changed to 115ms. Sending CAN data is normal, but there may be issues with receiving it? As per the first question.

0 Kudos
Reply
1 Reply

465 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个SBC 有驱动软件的,你自己下载从下面的链接:

DocStore :: Products (nxp.com)

0 Kudos
Reply