FS26: Why is the RSTB path check placed so late in the recommendation process?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26: Why is the RSTB path check placed so late in the recommendation process?

Jump to solution
608 Views
Kojimaa
Contributor III

Hi,

     This will increase the initialization time. Can I put this step at the forefront?

Kojimaa_0-1699867716090.png

Thank you in advance

 

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
542 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The reason why RSTB path check placed after fault error counter cleared is:

RSTB path check is suggested to perform when there is no error in the system. But it is not must to run RSTB path check at step4, you can adjust the sequence.

BR, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
543 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The reason why RSTB path check placed after fault error counter cleared is:

RSTB path check is suggested to perform when there is no error in the system. But it is not must to run RSTB path check at step4, you can adjust the sequence.

BR, Tomas

0 Kudos
Reply