Aurora Connector P2041

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Aurora Connector P2041

ソリューションへジャンプ
2,218件の閲覧回数
guillaume17
Contributor I

Hi,

I have a question about the Aurora connector of the P2041.

In document P2041 QorIQ Integrated Processor Hardware Specifications, Figure 58, SD_TX09_P and all others are not in "Table 1. Pin List by Bus".
Is this normal?

I may not have understood the SerDes use.


Thank you in advance

ラベル(1)
0 件の賞賛
返信
1 解決策
1,992件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is this normal?

This is "cut and paste" issue when the figures were taken from P3041 Hardware Specifications "as is", which is not correct for the P2041.

The P2041 has only one Debug/Aurora lane - Lane A in the SerDes Bank2 (SD_TX/RX[10])

The corrected Figure 58:

2018-04-13_131308.jpg

元の投稿で解決策を見る

1 返信
1,993件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is this normal?

This is "cut and paste" issue when the figures were taken from P3041 Hardware Specifications "as is", which is not correct for the P2041.

The P2041 has only one Debug/Aurora lane - Lane A in the SerDes Bank2 (SD_TX/RX[10])

The corrected Figure 58:

2018-04-13_131308.jpg